Tool/software:
Hello,team
We are using Ethernet to upgrade the image. In 1000M Ethernet mode, the transmission rate is only 6-8 MiB/s, which does not comply with the transmission rate of 1000M Ethernet. Why is the transmission so slow?
In the uboot environment, use the tftp command to transfer files:
=> tftp 0x82000000 aa link up on port 1, speed 1000, full duplex Using ethernet@8000000port@1 device TFTP from server 192.168.3.1; our IP address is 192.168.3.100 Filename 'aa'. Load address: 0x82000000 Loading: ##################T ################################ 128 MiB 6.8 MiB/s done Bytes transferred = 134217728 (8000000 hex) =>