This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

J784S4XEVM: errata queries

Part Number: J784S4XEVM

Tool/software:

Hello,

I am going through errata's of TI-j784S4 and would like to confirm below points.

https://www.ti.com/lit/er/sprz536b/sprz536b.pdf?ts=1724359040615&ref_url=https%253A%252F%252Fwww.google.com%252F

1. RAT : i2062
Is RAT module available/used for A72 core?

2. IA : i2196
It is not clear that workaround needs to be implemented in software(QNX on A51 core) or it is already taken care of/needs to take care at hardware level.

3. MSMC : i2378, i2381
Does this errata's are applicable if MSMC is configured as SRAM??

4. PCIe : i2242
Received or Derived ref clk mode, is it configurable at HW / SW level? If SW level, where I can confirm which mode is enabled? Any register to read?

PCIe :
MAIN_PLLx is in fractional or integer mode. Is it configurable at HW / SW level? If SW level, where I can confirm which mode is enabled? Any register to read?

5. UDMA : i2234
workaround says : This can be worked around by setting the EOL to 1 in the TR
What are the other impacts I should expect by setting EOL=1. Do I need to change any other configurations?

UDMA : i2146
Who handles/initiate forced teardown?I mean is it handled by ti library udma code? Can you confirm this?