Part Number: SK-TDA4VM
Tool/software:
Hi, experts
1.
There are some information about 4-CAN connectors but there isn't a detail demonstration about what 4-CANs are nor why 4-CANs are in SK-TDA4VM in the user manual. So I searched like this on web. Would you please correct if there is something not true information in here? Or if you have more information about the CANs, please let me know.
| CAN Interface | Function and Differences |
|---|---|
| MCU_CAN0 | - CAN interface connected to the MCU subsystem. - Mainly supports key MCU tasks like system management and safety functions. - Suitable for tasks requiring low latency and high reliability. |
| CAN5 | - General-purpose CAN interface connected to the SoC subsystem. - Handles typical communication tasks and can interface with various external devices. |
| CAN0 | - CAN interface connected to the main processor. - Supports application-level data exchange, such as sensor data collection and other diverse uses. |
| CAN9 | - CAN interface that can be used for applications requiring high-speed communication. - Provides similar functionality to CAN0 but supports additional expansion and high-speed communication. |
2.
I patched up like the articles. https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1334615/processor-sdk-j721e-can-driver-support-needed-for-a72-linux-of-processor-sdk-linux-sk-tda4vm/5119410?tisearch=e2e-sitesearch&keymatch=%25252520user%2525253A477602#5119410
0001-Enable-MCAN-for-SK-TDA4VM-on-6.1-kernel.patch
root@tda4vm-sk:/opt/edgeai-gst-apps# sudo ip link set can0 up root@tda4vm-sk:/opt/edgeai-gst-apps# root@tda4vm-sk:/opt/edgeai-gst-apps# lsmod | grep can can_raw 24576 0 can 24576 1 can_raw phy_can_transceiver 16384 4 m_can_platform 20480 0 m_can 36864 1 m_can_platform can_dev 45056 1 m_can root@tda4vm-sk:/opt/edgeai-gst-apps# ip link show type can 3: can0: <NOARP,UP,LOWER_UP,ECHO> mtu 16 qdisc pfifo_fast state UP mode DEFAULT group default qlen 10 link/can 4: can1: <NOARP,ECHO> mtu 16 qdisc noop state DOWN mode DEFAULT group default qlen 10 link/can 5: can2: <NOARP,ECHO> mtu 16 qdisc noop state DOWN mode DEFAULT group default qlen 10 link/can 6: can3: <NOARP,ECHO> mtu 16 qdisc noop state DOWN mode DEFAULT group default qlen 10
CAN0 : MCU_MCAN0
CAN1 : MCAN0
CAN2 : MCAN5
CAN3 : MCAN9
cansend can0 123#DEADBEEF
cansend can1 123#DEADBEEF
cansend can2 123#DEADBEEF
cansend can3 123#DEADBEEF
When connecting the CAN interfaces of one EVM (Evaluation Module) to another EVM, CAN communication is occurring at MCAN0/5/9 and signals are good.
But there is no signal on MCU_MCAN0.
In other CAN ports, the voltage level on H/L is approximately 2.4V in a standby state, but the MCU CAN port shows a level of 0V even when in standby. This suggests that the MCU CAN port might not be ready state for operating . What could be the reason for this?
3.
I connected the cables in a loop sequentially as CAN0 -CAN9 , CAN0-CAN5, or CAN0-MCU_CAN0.
After running the above command set and sending each connections, no signals were observed on any of the ports connection.
- Boot up the board and log in
- Initialize all 4 CAN interfaces:
ip link set can0 type can bitrate 1000000
ip link set can1 type can bitrate 1000000
ip link set can2 type can bitrate 1000000
ip link set can3 type can bitrate 1000000 - Turn all 4 CAN interfaces on:
ip link set can0 up
ip link set can1 up
ip link set can2 up
ip link set can3 up - Start listening on all 4 CAN interfaces:
candump can0 &
candump can1 &
candump can2 &
candump can3 & - Send a message from all 4 CAN interfaces:
cansend can0 123#DEADBEEF
cansend can1 123#DEADBEEF
cansend can2 123#DEADBEEF
cansend can3 123#DEADBEEF
Does the TI_SDK support looping like these?