Tool/software:
Hi TI support,
I am using AM6442 SK and I have enable CAN in Linux Kernel, but every time I reboot, I have to bring up the network interfaces manually, e.g.:
- ip link set can0 up type can bitrate 500000
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hi TI support,
I am using AM6442 SK and I have enable CAN in Linux Kernel, but every time I reboot, I have to bring up the network interfaces manually, e.g.:
- ip link set can0 up type can bitrate 500000
Hi,
In order to automate the process, you can use systemd service in linux to automatically run the required commands for establishing CAN communication.
An example: Unit Description=My Server StartLimitIntervalSec=0 Service Type=Simple ExecStart=/usr/sbin/1.sh Restart=always RestartSec=20 Install WantedBy=multi-user.target 1.sh → #!/bin/bash <insert commands> reboot sleep 1000 echo `date` >> /tmp/2
Regards,
Aparna
Hi,
You don't need to add this into an Yocto build.
1. Please add your .service file into the following location:
root@am62xx-evm:/etc/systemd/system# ls basic.target.wants graphical.target.wants bluetooth.target.wants local-fs.target.wants ctrl-alt-del.target multi-user.target.wants dbus-org.bluez.service network-online.target.wants dbus-org.freedesktop.Avahi.service sockets.target.wants dbus-org.freedesktop.network1.service sync-clocks.service dbus-org.freedesktop.resolve1.service sysinit.target.wants dbus-org.freedesktop.timesync1.service systemd-hostnamed.service dbus.service systemd-random-seed.service.wants default.target systemd-udevd.service getty.target.wants timers.target.wants root@am62xx-evm:/etc/systemd/system#
Then, you can auto run your service routine, by using the commands:
2. Now that the service file is in /etc/systemd/system folder, run the
following command to update System Daemon.
systemctl daemon-reload
3. To test that System Daemon, start the service by use the
following command:
systemctl start <name-of-sevice>.service
4. After test works, make the service autostart by using the following command:
systemctl enable <name-of-sevice>.service
Regards,
Aparna
Hi Aparna Patra,
Thank you for your answer!
But I have a large number of products, so I want to include it in the build so I can program it once into the product.
Hi,
Please refer: https://software-dl.ti.com/processor-sdk-linux/esd/AM62X/10_00_07_04/exports/docs/linux/Overview_Building_the_SDK.html
Regards,
Aparna