Tool/software:
Dear Sir,
I am currently working on the AM62x E3 Evolution Board, specifically with the AM6254 processor, and I’ve encountered a couple of issues that I need assistance with:
1. UART Input Issue:
I have successfully loaded the OS onto the board, and the kernel loading prints are visible in Tera Term.
However, the board is not accepting any input from my laptop’s keyboard. I am attempting to stop at U-Boot by pressing keys, but the input is not recognized.
I suspect this may be related to a Device Tree Source (DTS) configuration, but I am unsure of the exact cause or solution.
2. Wi-Fi Connectivity Issue:
After loading the OS, I noticed that Wi-Fi is not showing up as expected.
When running the #ifconfig command, the wlan0 interface is listed, but it fails to connect to any network.
I have verified that the Wi-Fi hardware is functioning, so I believe this could also be a configuration issue.
Could you please provide guidance on resolving these issues? Any insights into possible DTS misconfigurations or additional steps I should take to troubleshoot the Wi-Fi connectivity would be greatly appreciated.
Thank you for your support.
Best regards
Rajkumar