This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Re: AM18xx wi-fi EVM

I have the TMDXEVMWIFI1808L-A.

I have powered up the EVM using the linux SD card. Looks good, i get the standard menus.

From Here this is what i want to do:

1. Connect the EVM to a wi-fi network

I follow the instructions on the wiki and scan for networks. I double click the network i want to connect to and get the pop up. At this point i run into a problem, i cannot scroll to the end of the GUI to hit the "ADD" key after i enter the required fields. How do i scroll down? Is attaching a mouse the answer, or does the GUI need a scroll bar?