Other Parts Discussed in Thread: TMS320C6678
I want to run image processing on TMS320C6678 board。
Steps to Run the Demo
- Connect the board to a Ethernet hub or PC using Ethernet cable.
- The demo runs in Static IP mode if User Switch 1 is OFF else if it is ON then it runs in DHCP mode. See the Hardware Setup section for the location of User Switch 1.
- If it is configured in static IP mode, the board will come up with IP address 192.168.2.100, GW IP address 192.168.2.101 and subnet mask 255.255.254.0
- If it is configures in DHCP mode, it would send out DHCP request to get the IP address from a DHCP server in the network.
this is from “mcsdk_2_00_00_beta2/demos/image_processing/docs/image_processing_demonstration_user_guide.html”,
If it is configured in static IP mode,but I cann't find User Switch1, also cann't find the Hardware Setup section。