This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VE-Q1: How to change the multi codec demo decoding resolution on psdkra?

Part Number: TDA4VE-Q1


Tool/software:

Dear expert,

We have multi codec demo on openVX application. When I am testing the decoding feature on this demo, I encountered issue on decoding resolution. Pls take a look on how to change the decoding resolution on multi codec demo. Thanks .

1. Default demo, support 1920*1280, it works well.

2. When change to other resolution, like 720p or 1280*660 . Will encounter below issues.

APP: Init ... !!!
MEM: Init ... !!!
MEM: Initialized DMA HEAP (fd=5) !!!
MEM: Init ... Done !!!
IPC: Init ... !!!
IPC: Init ... Done !!!
REMOTE_SERVICE: Init ... !!!
REMOTE_SERVICE: Init ... Done !!!
    67.554849 s: GTC Frequency = 200 MHz
APP: Init ... Done !!!
    67.565737 s:  VX_ZONE_INIT:Enabled
    67.565803 s:  VX_ZONE_ERROR:Enabled
    67.565897 s:  VX_ZONE_WARNING:Enabled
    67.580071 s:  VX_ZONE_INIT:[tivxInitLocal:130] Initialization Done !!!
    67.591743 s:  VX_ZONE_INIT:[tivxHostInitLocal:101] Initialization Done for HOST !!!
Creating context done!
Kernel loading done!
app_init_display1 done 
BydAppInit Done!
Graph create done!
LDC Set Target done
Display1 Set Target done
BydAppCreateGraph Done!
BydAppSetGraph Done!
Graph verify done!
BydAppVerifyGraph Done!
gst_wrapper: GstCmdString:
filesrc location=./dlp_play_test_1280x720.mp4 
! qtdemux 
! h264parse 
! v4l2h264dec 
! videoconvert 
! video/x-raw, format=(string)NV12 
! tiovxmemalloc pool-size=7 
! appsink name=myAppSink0 drop=true wait-on-eos=false max-buffers=4

Codec Pipeline done!

appCodecSinkInit Done!
appCodecStart Done!
gst_wrapper: ERROR: TIOVX meta not found in pulled buffer!
gst_wrapper: exportgsttiovxbuffer FAILED!

(byd_hud_video_play.out:811): GStreamer-CRITICAL **: 17:42:59.510: gst_buffer_resize_range: assertion 'gst_buffer_is_writable (bufd

(byd_hud_video_play.out:811): GStreamer-WARNING **: 17:42:59.511: free_priv_data: object finalizing but still has parent (object:0)

(byd_hud_video_play.out:811): GStreamer-WARNING **: 17:42:59.511: free_priv_data: object finalizing but still has 1 parents (objec)

(byd_hud_video_play.out:811): GStreamer-CRITICAL **: 17:42:59.511: gst_mini_object_unlock: assertion 'state >= SHARE_ONE' failed

Regards,

Fredy Zhang