Hello,
I have a omap-l137\tms320c6747. I am trying to use it from a week but i am getting nowhere. I want to send the signal from the function generator to the line in and see the same signal in a oscilloscope from the line out port. If I understand this i can do the procesing stuff.
I need help in setting up for my seniour project. can somebody help me with this . if an agent can call and explain me that would be really helpfull and fast. so that I can understand what mistake is bieng done.
I have installed the software twice properly, tried to use the example but not able to get what these examples do.
Regards
Akshay