Part Number: PROCESSOR-SDK-AM64X
Tool/software:
Hi support,
I'm using the TI SDK release 09.02.01.10:
https://www.ti.com/tool/download/PROCESSOR-SDK-LINUX-AM64X/09.02.01.10

Test applied:
- Rebooting the Board_#1 by toggling the power supply on and off.
- 100Mbps line rate
- Each cycle of the poweroff/on test case is ~1min (10s reboot, <1min to setup HSR after reboot)
Trouble-shooting:
Board_#2 is AM64x EVM board, left on the picture. Board_#3 is project specific board right on the picture.
- profishark sniffing traffic: Board_#2 didn’t forward incoming packets from port B to A, Board_#3 didn’t forward incoming packets from port A to B.
- The HSR supervision A packets of Board_#1 and Board_#3 were transmitted into #2.B but were not found in #2.A outgo.
- The HSR supervision B packets of Board_#1 and Board_#2 were transmitted into #3.A but were not found in #3.B outgo.
- Ethtool -S: the pru ports “rx_min_size_error_frames” of Board_#2 and Board_#3 were significantly increased abnormally.
IMPORTANT: Issue is reproduced only if board Board_#1 is power off/on. Period between off/on is 10s. If we are doing reboot from Linux with command reboot, issue is not reproduced after 24h.