Part Number: AM69
Tool/software:
Hello TI Experts,
We have a custom HW based on AM69. Would like to validate the thermal profiling of the HW with a full load on CPUs and all 4 C7x (32 TOPS) + MMA accelerators available on SOC.
Seems like below demo/utility from the TI RTOS SDK's Vision Apps is relevant for our use-case, however as far as I understand, Linux + RTOS SDK is not supported on AM69.
How can we enable these RTOS demos on AM69 device ?
Just to note that with `ti-rtos-firmware` recipe for C7x firmware, we are able to see all 4 C7x DSP cores (32 TOPS) up and running on our platform.
Would need help/support for the demos/utilities which can simulate load on each C7x + MMA.
root@aquila-am69-02242602:~# cat /sys/class/remoteproc/remoteproc*/name 64800000.dsp 65800000.dsp 5e00000.r5f 66800000.dsp 5f00000.r5f 67800000.dsp 5900000.r5f 5a00000.r5f root@aquila-am69-02242602:~# cat /sys/class/remoteproc/remoteproc*/state running running running running running running running running
Thank you.
Regards,
Parth P