This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM365 reboot when starting network operation (a new hardware)



Dear All:

 

There is a hardware question.

Our customer design a new DM365 board.

We are testing it.

It can boot from SD or NAND successfully. to u-boot.

It can also boot to Linux kernel (SDK3).

However, whenever we do any network operation, such as ping in u-boot,

it will reboot the system immediately. (even after we get ride of the Phy)

We checked the DDR and it seemed to be OK.

Someone told us it may be caused by a power problem.

We'd like to confirm this possibility to help our customer to continue their debug procedure.

Any comment will be welcome.

 

best regards,

 

Ray