Hi,
I have read in the Hardware Migration Guide (http://processors.wiki.ti.com/index.php/OMAP35x_To_AM37x_Hardware_Migration_Guide) that there was a change relating on the handling with the gpios 120 - 129.
On our board we have used the following configuration for the GPIO_129:
Mux.h: CONTROL_PADCONF_GPIO_129 0x0A5A
board-config.h: MUX_VAL(CP(GPIO_129), (IDIS | PTU | DIS | M4))
Also the CONTROL_PBIAS_LITE register is configured correctly.(The PBIASLIGHTPWRDNZ1 Bit is set to 1).
However, I can't measure an output signal on the GPIO_129 pin.
I also used for example GPIO_139 with the following settings:
mux.h: CONTROL_PADCONF_MMC2_DAT7 0x016A
board-config.h: MUX_VAL(CP(MMC2_DAT7), (IDIS | PTD | DIS | M4))
In this case the configuration works correct, and there can be measured an output signal.
Has someone an idea, why my GPIO_129 configuration doesn't work?
Thanks in advance,
Best Regards
Christian