This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM6446 EVM Demo issue

Hi,

When i run my 6446EVM booting from flash to run the demo as standalone i get the interfcae screen but when i choose any demo using the ir-remote i get nothing happen i can choose any demo but when i press play the screen go to black for a part of second and return back to its state that shows the player keys without happen any thing

my 6446EVM starting output is as follow there is some errors on it i mark it in yellow please ana one can help me

DM644x initialization passed!
TI UBL Version: 1.50
Booting Catalog Boot Loader
BootMode = NOR
Starting NOR Copy...
CFI Query...passed.
NOR Initialization:
        Command Set: Intel
        Manufacturer: INTEL
        Size: 0x00000010 MB
   DONE
Jumping to entry point at 0x81080000.


U-Boot 1.2.0 (May 20 2009 - 01:04:51)

I2C:   ready
DRAM:  256 MB
INTEL Flash: 16 MB
In:    serial
Out:   serial
Err:   serial
ARM Clock :- 297MHz
DDR Clock :- 162MHz
MSP430 Firmware supports AM/PM Feature
Hit any key to stop autoboot:  0
## Booting image at 02060000 ...
   Image Name:   Linux-2.6.18_pro500-davinci_evm-
   Image Type:   ARM Linux Kernel Image (uncompressed)
   Data Size:    2018280 Bytes =  1.9 MB
   Load Address: 80008000
   Entry Point:  80008000
   Verifying Checksum ... OK
OK

Starting kernel ...

Uncompressing Linux.....................................................................................................
................................ done, booting the kernel.
Linux version 2.6.18_pro500-davinci_evm-arm_v5t_le (x0029463@aspbuild11) (gcc version 4.2.0 20070126 (prerelease) (Monta
Vista 4.2.0-3.0.0.0702771 2007-03-10)) #1 PREEMPT Wed May 20 01:14:17 IST 2009
CPU: ARM926EJ-S [41069265] revision 5 (ARMv5TEJ), cr=00053177
Machine: DaVinci EVM
Memory policy: ECC disabled, Data cache writeback
DaVinci DM6443 variant 0x1
CPU0: D VIVT write-back cache
CPU0: I cache: 16384 bytes, associativity 4, 32 byte lines, 128 sets
CPU0: D cache: 8192 bytes, associativity 4, 32 byte lines, 64 sets
Built 1 zonelists.  Total pages: 30720
Kernel command line: video=davincifb:vid0=0,2500K:vid1=0,2500K:osd0=720x480x16,1350K@0,0:osd1=720x480x16,1350K@0,0 davin
ci_enc_mngr.ch0_output=COMPOSITE davinci_enc_mngr.ch0_mode=NTSC console=ttyS0,115200n8 noinitrd ip=192.168.1.41:192.168.
1.1:255.255.255.0:192.168.1.2:192.168.1.3::off root=/dev/hda1 mem=120M
PID hash table entries: 512 (order: 9, 2048 bytes)
Clock event device timer0_0 configured with caps set: 03
Console: colour dummy device 80x30
Dentry cache hash table entries: 16384 (order: 4, 65536 bytes)
Inode-cache hash table entries: 8192 (order: 3, 32768 bytes)
Memory: 120MB = 120MB total
Memory: 117376KB available (3461K code, 689K data, 176K init)
Security Framework v1.0.0 initialized
Capability LSM initialized
Mount-cache hash table entries: 512
CPU: Testing write buffer coherency: ok
NET: Registered protocol family 16
DaVinci: 71 gpio irqs
WARNING: both IDE and NOR flash are enabled, but share pins.
        Disable IDE for NOR support.
ch0 default output "COMPOSITE", mode "NTSC"
MUX: initialized LOEEN
MUX: initialized LFLDEN
VPBE Encoder Initialized
LogicPD encoder initialized
SCSI subsystem initialized
usbcore: registered new driver usbfs
usbcore: registered new driver hub
NET: Registered protocol family 2
IP route cache hash table entries: 1024 (order: 0, 4096 bytes)
TCP established hash table entries: 4096 (order: 2, 16384 bytes)
TCP bind hash table entries: 2048 (order: 1, 8192 bytes)
TCP: Hash tables configured (established 4096 bind 2048)
TCP reno registered
davinci_spi_board_init: NO spi support
VFS: Disk quotas dquot_6.5.1
Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
squashfs: version 3.1 (2006/08/19) Phillip Lougher
JFFS2 version 2.2. (NAND) (C) 2001-2006 Red Hat, Inc.
yaffs May 20 2009 01:11:27 Installing.
SGI XFS with no debug enabled
Initializing Cryptographic API
io scheduler noop registered
io scheduler anticipatory registered (default)
LTT : ltt-facilities init
LTT : ltt-facility-core init in kernel
davincifb davincifb: dm_osd0_fb: 720x480x16@0,0 with framebuffer size 1350KB
davincifb davincifb: dm_vid0_fb: 0x0x16@0,0 with framebuffer size 2500KB
davincifb davincifb: dm_osd1_fb: Initial window configuration is invalid.
davincifb davincifb: dm_osd1_fb: 720x480x16@0,0 with framebuffer size 1350KB
davincifb davincifb: dm_vid1_fb: 0x0x16@0,0 with framebuffer size 2500KB
davincifb davincifb.0: dm_osd0_fb: Failed to obtain ownership of OSD window.
DAVINCI-WDT: DaVinci Watchdog Timer: heartbeat 60 sec
Serial: 8250/16550 driver $Revision: 1.90 $ 2 ports, IRQ sharing disabled
serial8250.0: ttyS0 at MMIO map 0x1c20000 mem 0xfec20000 (irq = 40) is a 16550A
RAMDISK driver initialized: 1 RAM disks of 32768K size 1024 blocksize
netconsole: not configured, aborting
TI DaVinci EMAC: MAC address is 00:0e:99:02:43:83
TI DaVinci EMAC Linux version updated 4.0
TI DaVinci EMAC: Installed 1 instances.
Linux video capture interface: v2.00
vpfe vpfe.1: DaVinci v4l2 capture driver V1.0 loaded
Trying to register davinci display video device.
layer=c0d36600,layer->video_dev=c0d36760
Trying to register davinci display video device.
layer=c0d36400,layer->video_dev=c0d36560
davinci_init:DaVinci V4L2 Display Driver V1.0 loaded

 Davici AEW Driver cannot be loaded
 VIDEO PORT is not enabledData Flow path from CCDC is disabled

 Davinci AF driver cannot be loaded
 VIDEO PORT is not enabled
 CCDC needs to be configured<6>i2c /dev entries driver
Uniform Multi-Platform E-IDE driver Revision: 7.00alpha2
ide: Assuming 50MHz system bus speed for PIO modes; override with idebus=xx
MUX: initialized HDIREN
MUX: initialized ATAEN
    ide0: MMIO-DMA , BIOS settings: hda:pio, hdb:pio
hda: TOSHIBA MK4032GAX, ATA DISK drive
ide0 at 0xfec661f0-0xfec661f7,0xfec663f6 on irq 22
hda: max request size: 512KiB
hda: 78140160 sectors (40007 MB), CHS=16383/255/63, UDMA(66)
hda: cache flushes supported
 hda: hda1 hda2
Initializing USB Mass Storage driver...
usbcore: registered new driver usb-storage
USB Mass Storage support registered.
usbcore: registered new driver usbhid
drivers/usb/input/hid-core.c: v2.6:USB HID core driver
musb_hdrc: version 6.0, cppi-dma, host, debug=0
musb_hdrc musb_hdrc: No DMA interrupt line
musb_hdrc: USB Host mode controller at c805e000 using DMA, IRQ 12
musb_hdrc musb_hdrc: MUSB HDRC host driver
musb_hdrc musb_hdrc: new USB bus registered, assigned bus number 1
usb usb1: configuration #1 chosen from 1 choice
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 1 port detected
mice: PS/2 mouse device common for all mice
rtc_davinci_evm rtc_davinci_evm: rtc intf: proc
rtc_davinci_evm rtc_davinci_evm: rtc intf: dev (254:0)
rtc_davinci_evm rtc_davinci_evm: rtc core: registered rtc_davinci_evm as rtc0
rtc0: hours 12-23 are misreported as duplicate hours 00-11
davinci-mmc davinci-mmc.0: Supporting 4-bit mode
davinci-mmc davinci-mmc.0: Using DMA mode
Advanced Linux Sound Architecture Driver Version 1.0.12rc1 (Thu Jun 22 13:55:50 2006 UTC).
ASoC version 0.13.1
MUX: initialized MCBSP
AIC3X Audio Codec 0.1
asoc: aic3x <-> davinci-i2s mapping ok
ALSA device list:
  #0: DaVinci EVM (aic3x)
IPv4 over IPv4 tunneling driver
TCP bic registered
NET: Registered protocol family 1
NET: Registered protocol family 17
Time: timer0_1 clocksource has been installed.
Clock event device timer0_0 configured with caps set: 08
Switched to high resolution mode on CPU 0
rtc_davinci_evm rtc_davinci_evm: setting the system clock to 2004-02-01 12:16:14 (1075637774)
IP-Config: Unable to set interface netmask (-22).
kjournald starting.  Commit interval 5 seconds
EXT3-fs warning: maximal mount count reached, running e2fsck is recommended
EXT3 FS on hda1, internal journal
EXT3-fs: mounted filesystem with ordered data mode.
VFS: Mounted root (ext3 filesystem).
Freeing init memory: 176K
INIT: version 2.86 booting
Starting the hotplug events dispatcher: udevd.
Synthesizing the initial hotplug events...done.
Waiting for /dev to be fully populated...done.
Activating swap...done.
Remounting root filesystem...done.
Calculating module dependencies
WARNING: Couldn't open directory /lib/modules/2.6.18_pro500-davinci_evm-arm_v5t_le: No such file or directory
FATAL: Could not open /lib/modules/2.6.18_pro500-davinci_evm-arm_v5t_le/modules.dep.temp for writing: No such file or di

rectory
Loading modules:
Checking all file systems: fsck
fsck 1.40 (29-Jun-2007)
Mounting local filesystems: mount nothing was mounted
Setting up networking ....
/etc/network/options is deprecated.
Setting up IP spoofing protection: rp_filter done.
Disabling IPv4 packet forwarding: done.
Disabling TCP/IP Explicit Congestion Notification: done.
Starting network interfaces: done.
Starting hotplug subsystem:
   pci
   pci      [success]
   usb
   usb      [success]
   isapnp
   isapnp   [success]
   ide
   ide      [success]
   input
   input    [success]
   scsi
   scsi     [success]
done.
Starting portmap daemon....
Cleaning: /tmp /var/lock /var/run done.
Updating /etc/motd...done.
INIT: Entering runlevel: 3
Starting system log daemon: syslogd klogd.
Starting NFS common utilities: statd.
Starting internet superserver: inetd.
Starting OpenBSD Secure Shell server: sshd.
CMEMK module: built on May 26 2009 at 09:30:32
  Reference Linux version 2.6.18
  File /db/atree/library/trees/linuxdemos/linuxdemos-d28x/imports/DEMO_common/linuxutils_2_23_01/packages/ti/sdo/linuxut
ils/cmem/src/module/cmemk.c
CMEMK Error: CMEM phys_start (0x87600000) overlaps kernel (0x80000000 -> 0x87800000)
insmod: error inserting 'cmemk.ko': -1 Invalid parameters
dsplinkk: no version for "struct_module" found: kernel tainted.

DSPLINK Module (1.61.03) created on Date: May 26 2009 Time: 09:35:23
Starting web server ...
 thttpd

MontaVista(R) Linux(R) Professional Edition 5.0.0 (0801921)

192 login: