This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Facing problem in Network initialization on C6678 EVM



I have a simple multi-core application wherein I initilize netowrk and  communicate with PC over the network. I got following error upon running:

[C66xx_0] EVM in StaticIP mode at 192.168.10.12

[C66xx_0] Set IP address of PC to 192.168.10.10

[C66xx_0] Error opening a PA Command Response queue

[C66xx_0] PASS init failed

I am using following versions:

bios_6_32_04_49, mcsdk_2_00_02_14, ndk_2_20_04_26 and pdk_C6678_1_0_0_14.

Could anybody please help me out to resolve this issue.