This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SK-AM62B-P1: Issue with configuring PWM through the User Expansion Connector

Part Number: SK-AM62B-P1

Tool/software:

Hi TI,

I'm using SK-AM62B-P1 running on Debian bookworm. I was trying to get a PWM output of 50% duty cycle from pin number 33 which is the EXP_EHRPWM1_B. But I don't see anything on the /sys/class/pwm/

Here is the output for the same : 

On my research, as per PWM I understood that PWM drivers are missing in the Kernal space. So how should I proceed on this? Do I need to build a new Kernal? or can I add the PWM drivers (eHRPWM and eCAP) as loadable kernal modules?

Also, is there any kernal configuration tools (menuconfig, defconfig) available ready out of the box in the debian bookworm?