Tool/software:
Dear All,
we have a input PPS signal and Input 10MHz clk. we want to use CPTS module to generate output trigger signal for a sensor.
We connected input PPS to MCU_CPTS0_HW2TSPUSH ( MCU domain) or CPTS0_HW2TSPUSH ( main domain)
We connected input 10MHz clk to MCU_CPTS0_RFT_CLK ( MCU domain) or CPTS0_RFT_CLK ( main domain)
On what pin can we generate the output signal ( where should we route the TS_GENFn) ?
1) In MCU domain , can we rout it to
-> MCU_TIMER_IO1 pin (B26)
-> SYNC0_OUT (AB26)
-> SYNC1_OUT (AD28)
-> SYNC2_OUT (T28)
-> SYNC3_OUT (Y27)
2) In MAIN domain , can we rout it to
-> TIMER_IO1 pin (AG25)
-> SYNC0_OUT (AB26)
-> SYNC1_OUT (AD28)
-> SYNC2_OUT (T28)
-> SYNC3_OUT (Y27)
3) Or are there any other option to do this?
Best Regards,
d.