This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Building the H264 codec sample test application



Hi,

I am trying to build the sample test application that came along with the TI H264 codec, version 2_00_004, for the DM6446.

I initially got an error message "can't find input file 'dman3d.a64P' ". I fixed this by modifying the .pjt file to point to debug/dman3.a64P.

I now get the following error messages 

 

>> warning: creating output section $build.attributes without SECTIONS specification

>> internal error: ABBREV_TABLE::find_decl: decl_map is not available

How do i fix this issue?

I am using CCS  3.3.82.13, bios 5.32.04 and framework components 2.21.

 

Thanks,

Arun