Hi all
I just want to make sure if the codec can only decode H.264 by frame(or by stream is ok?).
Regards
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi all
I just want to make sure if the codec can only decode H.264 by frame(or by stream is ok?).
Regards
Hi,
Which platform are you referring to?
Could you be a little more clear on decode by frame and decode by stream
sorry for the bad description.My platform is DM6467.
I have two board and using socket to trasnmit H.264 stream. And I cut the stream into some pieces for UDP transmition, so each piece is incomplete.
Can i give the Vdec_process by piece? or I should put the pieces together first?
DM6467 codec needs min 1 frame of data to be avialable for encode or decode. It does not support6 subframe processing APIs. So, you need to put the pieces together to make it at least 1 frame worth data.
regards
Yashwant