This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

What are the differences between ARAGO filesystem and EZSDK filesystem?

What are the differences between ARAGO filesystem and EZSDK filesystem?

EZSDK_5_02_02_60 is used to develop the application. In EZSDK, there are two root filesystems such as aragoXXX.tar.gz and ezsdkXXX.tar.gz.

For 128MB NAND flash, ARAGO filesystem is fitted into my NAND flash,but EZSDK is not acceptable because the latter is too  big.

I want to move  binaries, scripts and libraries from EZSDK filesystem to ARAGO filesystem. Is it possible?

Can you explain the details of both filesystems?