Hello,
I try to boot the AM3517 evaluation board using NOR flash.
To prepare X-Loader, U-Boot and configure S11 and S7 switches, I had used "AM35x-NOR-Flash-Support-ApplicationNote".
I've got many question about this application note :
1) "EVM Board modification (NOR Boot mode) -> From SOM board remove R235 register."
=> R235 is a resistor connected to combo (no relationship with NOR or NAND flashes !). Is this information is valid ? Do I have to remove another resistor ?
2) "NOR flash boot mode doesn't work with an application board < Rev4 revision due to hardware issue"
=> Where can I find this revision identifier in application board (mine seems to be set to "1014698 Rev. A") ?
3) Do I have to sign the "x-load.bin" file before downloading it in NOR flash ?
Thanks a lot for your help,
Jean-Marc.