This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

8168 EVM (DDR3) Hardware User Guide

Hi

1. I use EVM 8168 DDR3. 8168 EVM Hardware User Guides are not included in SD card. Please any TI links where I can download

2. For android porting on EVM 8168 DDR3, which android version should be used? what is procedure for android porting. I am very new in Android.

3. 7 inch LCD monitor is provided with 8168 DDR3 EVM, is it touch screen LCD? Do I need to install Touch Kit driver ( provided in CD) to make it touch screen

4. How is procedure to test  RGB & S-video outputs (Base board). Is there sample applications in SDK to test RGB and s-video?

 

Regards

Soibam