Other Parts Discussed in Thread: AM4376, TPS65216
Tool/software:
Hi
We are developing the custom board with AM4376 based on AM437x-EVM.
SDK : PROCESSOR-SDK-AM437X-06.03.00.106
To fix the frequency to 1GHz, we changed the device tree as below.
dcdc2: regulator-dcdc2 {
regulator-name = "vdd_mpu";
- regulator-min-microvolt = <912000>;
- regulator-max-microvolt = <1378000>;
+ regulator-min-microvolt = <1298500>;
+ regulator-max-microvolt = <1351500>;
regulator-boot-on;
regulator-always-on;
};
This change is causes the automatic reboot after we execute the "poweroff" command.
Before this change, the "poweroff" command works normally.
(No automatic reboot.)
Could you please let us know why this change causes this issue?
We are using TPS65216 as PMIC. It is changed from AM437x-EVM.
Thanks.
Best regards,