This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VH-Q1: how to solve CSI Fvid2Utis_dequeue error in tda4-vh?

Part Number: TDA4VH-Q1

Tool/software:

hi,brijesh,
In the current power-on and power-off aging test on the vh platform, there is a low probability that csirx enqueue buffer fail during the running process.
Related printing:
"src/csirx_drv.c @ Line 599: ALLOC: Q object allocation failed"
Check the sdk code and find that Fvid2Utis_dequeue returns a null pointer, CSIRX_CAPT_QUEUE_DEPTH_PER_CH is 10, the project has only two cameras, a total of 8 buffers, when the error is enqueue two buffers in turn. There is no more than 10. Please ask experts to help analyze the cause of this problem. Can we add any logic to locate it?

cam info: two raw 12 cam , 10 hz.

zyt,

jovan