Part Number: PROCESSOR-SDK-AM62X
Other Parts Discussed in Thread: SK-AM62B-P1
Tool/software:
Hi ti ,
Please find the RAM inside my system using free command
# free
total used free shared buff/cache available
Mem: 1970924 62260 1795772 13560 112892 1826180
when i run test with 512M its getting passed without issues
But when i run ram test with 1G getting kernel panic and halted. is it expcted ?
root@am62xx-evm:~# memtester 1G 1 memtester version 4.5.1 (64-bit) Copyright (C) 2001-2020 Charles Cazabon. Licensed under the GNU General Public License version 2 (only). pagesize is 4096 pagesizemask is 0xfffffffffffff000 want 1024MB (1073741824 bytes) got 1024MB (1073741824 bytes), trying mlock ...[ 173.124184] Unable to handle kernel NULL pointer 8 [ 173.132997] Mem abort info: [ 173.135779] ESR = 0x0000000096000046 [ 173.139517] EC = 0x25: DABT (current EL), IL = 32 bits [ 173.144817] SET = 0, FnV = 0 [ 173.147862] EA = 0, S1PTW = 0 [ 173.150992] FSC = 0x06: level 2 translation fault [ 173.155858] Data abort info: [ 173.158726] ISV = 0, ISS = 0x00000046 [ 173.162550] CM = 0, WnR = 1 [ 173.165507] user pgtable: 4k pages, 48-bit VAs, pgdp=0000000086563000 [ 173.171934] [0000000000000008] pgd=0800000081d9a003, p4d=0800000081d9a003, pud=080000008169e003, 0 [ 173.182540] Internal error: Oops: 0000000096000046 [#1] PREEMPT SMP [ 173.188795] Modules linked in: rpmsg_ctrl rpmsg_char dwc3 crct10dif_ce overlay ti_k3_r5_remotepro6 [ 173.211086] CPU: 0 PID: 500 Comm: memtester Tainted: G O 6.1.33-g40c32565ca #1 [ 173.219682] Hardware name: Texas Instruments AM625 SK TESSS (DT) [ 173.225675] pstate: 800000c5 (Nzcv daIF -PAN -UAO -TCO -DIT -SSBS BTYPE=--) [ 173.232626] pc : get_page_from_freelist+0x228/0xf10 [ 173.237512] lr : get_page_from_freelist+0x1d0/0xf10 [ 173.242382] sp : ffff800009ff3840 [ 173.245685] x29: ffff800009ff3840 x28: 0000000000000801 x27: ffff8000091e80c0 [ 173.252814] x26: ffffffffffffffff x25: 0000000000000000 x24: fffffc000021f900 [ 173.259943] x23: 0000000000000000 x22: 0000000000000000 x21: ffff0000772f0718 [ 173.267071] x20: ffff0000772f0700 x19: ffff0000772f0700 x18: 000000000004773e [ 173.274199] x17: 0000000000000000 x16: ffff800008ca3330 x15: 0000000000000000 [ 173.281328] x14: 0000000000000001 x13: 0000000000000002 x12: 0000000000000010 [ 173.288455] x11: fffffc0000d68000 x10: 0000000000000200 x9 : fffffc0000348008 [ 173.295584] x8 : 0000000000000000 x7 : 0000000000000001 x6 : 00000000000000c0 [ 173.302712] x5 : 00000000ffffffff x4 : 0000000000000000 x3 : dead000000000122 [ 173.309840] x2 : 0000000000000000 x1 : fffffc000021f908 x0 : ffff0000772f0718 [ 173.316969] Call trace: [ 173.319409] get_page_from_freelist+0x228/0xf10 [ 173.323933] __alloc_pages+0x134/0xcec [ 173.327676] __pte_alloc_one.constprop.0+0x28/0x90 [ 173.332464] do_huge_pmd_anonymous_page+0x200/0x7f0 [ 173.337336] __handle_mm_fault+0x420/0xc00 [ 173.341426] handle_mm_fault+0xec/0x280 [ 173.345254] __get_user_pages+0x200/0x3a0 [ 173.349261] populate_vma_page_range+0x58/0x7c [ 173.353695] __mm_populate+0xb4/0x190 [ 173.357348] do_mlock+0xcc/0x250 [ 173.360570] __arm64_sys_mlock+0x18/0x30 [ 173.364485] invoke_syscall+0x48/0x114 [ 173.368232] el0_svc_common.constprop.0+0xd4/0xfc [ 173.372929] do_el0_svc+0x30/0xd0 [ 173.376238] el0_svc+0x2c/0x84 [ 173.379294] el0t_64_sync_handler+0xbc/0x140 [ 173.383558] el0t_64_sync+0x18c/0x190 [ 173.387220] Code: d2802443 f2fbd5a3 d1002038 a9400022 (f9000440) [ 173.393301] ---[ end trace 0000000000000000 ]--- [ 173.397908] note: memtester[500] exited with irqs disabled [ 173.403496] note: memtester[500] exited with preempt_count 2 [ 173.409290] Unable to handle kernel NULL pointer dereference at virtual address 0000000000000038 [ 173.418058] Mem abort info: [ 173.420840] ESR = 0x0000000096000006 [ 173.424577] EC = 0x25: DABT (current EL), IL = 32 bits [ 173.429877] SET = 0, FnV = 0 [ 173.432920] EA = 0, S1PTW = 0 [ 173.436050] FSC = 0x06: level 2 translation fault [ 173.440914] Data abort info: [ 173.443784] ISV = 0, ISS = 0x00000006 [ 173.447607] CM = 0, WnR = 0 [ 173.450564] user pgtable: 4k pages, 48-bit VAs, pgdp=0000000081ef3000 [ 173.456991] [0000000000000038] pgd=0800000081eda003, p4d=0800000081eda003, pud=0800000081ed9003, 0 [ 173.467590] Internal error: Oops: 0000000096000006 [#2] PREEMPT SMP [ 173.473842] Modules linked in: rpmsg_ctrl rpmsg_char dwc3 crct10dif_ce overlay ti_k3_r5_remotepro6 [ 173.496113] CPU: 0 PID: 150 Comm: systemd-journal Tainted: G D O 6.1.33-g40c32565ca1 [ 173.505229] Hardware name: Texas Instruments AM625 SK TESSS (DT) [ 173.511220] pstate: 400000c5 (nZcv daIF -PAN -UAO -TCO -DIT -SSBS BTYPE=--) [ 173.518170] pc : kmem_cache_alloc+0x17c/0x3f0 [ 173.522521] lr : kmem_cache_alloc+0x80/0x3f0 [ 173.526783] sp : ffff80000961bbd0 [ 173.530086] x29: ffff80000961bbd0 x28: ffff000001cdd140 x27: ffff8000090ea000 [ 173.537215] x26: 0000000000000000 x25: ffff000000f91c80 x24: 0000000000000001 [ 173.544343] x23: ffff000000014a00 x22: ffff0000016c2380 x21: ffff000001cdd0a0 [ 173.551471] x20: 0000000000000a20 x19: 0000000000000000 x18: ffff80000961bd68 [ 173.558599] x17: 0000000000000000 x16: ffff800008ca3330 x15: 0000000000000000 [ 173.565728] x14: ffff000001f2a20c x13: 1fffe000003e5441 x12: ffff80000961bd68 [ 173.572856] x11: 0000000000000000 x10: ffff000001f2a208 x9 : 0000000000000001 [ 173.579984] x8 : 0000000000000001 x7 : ffff80006e33c000 x6 : 0000000000000618 [ 173.587112] x5 : 0000000000000919 x4 : ffff0000772f0a60 x3 : 0000000000029700 [ 173.594240] x2 : 0000000000000028 x1 : ffffffffffffffff x0 : 0000000000000000 [ 173.601368] Call trace: [ 173.603805] kmem_cache_alloc+0x17c/0x3f0 [ 173.607807] __sigqueue_alloc+0x80/0x130 [ 173.611724] __send_signal_locked.part.0+0x1ec/0x2e0 [ 173.616680] send_signal_locked+0x84/0x14c [ 173.620769] force_sig_info_to_task+0xec/0x130 [ 173.625205] force_sig_fault+0x50/0x7c [ 173.628946] arm64_force_sig_fault+0x40/0x70 [ 173.633213] do_page_fault+0x380/0x3d0 [ 173.636959] do_translation_fault+0xac/0xc0 [ 173.641135] do_mem_abort+0x44/0x94 [ 173.644618] el0_da+0x30/0x90 [ 173.647582] el0t_64_sync_handler+0xf8/0x140 [ 173.651846] el0t_64_sync+0x18c/0x190 [ 173.655504] Code: 9a810273 f9400260 7217001f 9a9f1273 (f9401e60) [ 173.661583] ---[ end trace 0000000000000000 ]--- [ 173.666187] note: systemd-journal[150] exited with irqs disabled [ 173.672221] note: systemd-journal[150] exited with preempt_count 1
Kindly help me on this as it is crititcal to us
Thanks,
Naresh