Other Parts Discussed in Thread: AM3517
Hello,
I want to use single-chip DDR2 memory with the 3517.
In the am3517.pdf datasheet (6.4.2.1.1, page 130) there is an explanation on how to use 1x16 LPDDR with the AM3517.
In the clause 6.4.2.2.1, however, there is no equivalent note on 1x16 DDR2 use.
- Is this mode not supported at all?
- If it is supported, do I need to update anything in the linux kernel?
Thanks.