This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM625: follow-up GPIO behavior when resuming from the Deep Sleep mode

Part Number: AM625


Tool/software:

This is a follow-up of this thread: https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1392583/am625-unexpected-gpio-behavior-when-resuming-from-the-deep-sleep-mode/5335912#5335912

The patch provided there by was applied and worked as there was no drop in the measured GPIO state when resuming from deep sleep.

without patch:

with:

Log during measurement:

U-Boot SPL 2024.04-ti-gffbbc1dd68f4 (Aug 28 2024 - 11:52:19 +0000)
SYSFW ABI: 4.0 (firmware rev 0x000a '10.0.8--v10.00.08 (Fiery Fox)')
Changed A53 CPU frequency to 1250000000Hz (T grade) in DT
SPL initial stack usage: 13424 bytes
Trying to boot from MMC1
Authentication passed
Authentication passed
Authentication passed
Loading Environment from nowhere... OK
init_env from device 9 not supported!
Authentication passed
Authentication passed
Starting ATF on ARM64 core...

NOTICE:  BL31: v2.11.0(release):v2.11.0-dirty
NOTICE:  BL31: Built : 11:51:22, May 23 2024

U-Boot SPL 2024.04-ti-gffbbc1dd68f4 (Aug 28 2024 - 11:52:19 +0000)
SYSFW ABI: 4.0 (firmware rev 0x000a '10.0.8--v10.00.08 (Fiery Fox)')
SPL initial stack usage: 1904 bytes
Trying to boot from MMC1
Authentication passed
Authentication passed


U-Boot 2024.04-ti-gffbbc1dd68f4 (Aug 28 2024 - 11:52:19 +0000)

SoC:   AM62X SR1.0 HS-FS
DRAM:  2 GiB
Core:  145 devices, 31 uclasses, devicetree: separate
MMC:   mmc@fa10000: 0, mmc@fa00000: 1
Loading Environment from MMC... OK
MISSING TORADEX CARRIER CONFIG BLOCKS
In:    serial@2800000
Out:   serial@2800000
Err:   serial@2800000
Model: Toradex 0076 Verdin AM62 Quad 2GB WB IT V1.2A
Serial#: 15412844
am65_cpsw_nuss ethernet@8000000: K3 CPSW: nuss_ver: 0x6BA01103 cpsw_ver: 0x6BA81103 ale_ver: 0x00290105 Ports:2
Setting variant to wifi
Net:   
Warning: ethernet@8000000port@1 MAC addresses don't match:
Address in ROM is               98:03:8a:76:36:f6
Address in environment is       00:14:2d:eb:2e:6c
eth0: ethernet@8000000port@1 [PRIME]Could not get PHY for mdio@f00: addr 7
am65_cpsw_nuss_port ethernet@8000000port@2: phy_connect() failed

Hit any key to stop autoboot:  0 
MMC: no card present
switch to partitions #0, OK
mmc0(part 0) is current device
Scanning mmc 0:1...
Found U-Boot script /boot.scr
6085 bytes read in 11 ms (540 KiB/s)
## Executing script at 90280000
Loading DeviceTree: k3-am625-verdin-wifi-dev.dtb
71555 bytes read in 11 ms (6.2 MiB/s)
98 bytes read in 10 ms (8.8 KiB/s)
Working FDT set to 90200000
Applying Overlay: verdin-am62_panel-cap-touch-10inch-lvds_overlay.dtbo
5314 bytes read in 13 ms (398.4 KiB/s)
Applying Overlay: verdin-am62_spidev_overlay.dtbo
560 bytes read in 11 ms (48.8 KiB/s)
8207976 bytes read in 64 ms (122.3 MiB/s)
Bootargs: root=PARTUUID=c4e4fc06-02 ro rootwait console=tty1 console=ttyS2,115200
   Uncompressing Kernel Image to 0
## Flattened Device Tree blob at 90200000
   Booting using the fdt blob at 0x90200000
Working FDT set to 90200000
   Loading Device Tree to 0000000098eb0000, end 0000000098ee4fff ... OK
Working FDT set to 98eb0000

Starting kernel ...

[    0.000000] Booting Linux on physical CPU 0x0000000000 [0x410fd034]
[    0.000000] Linux version 6.6.32-gda8dd76693a4-dirty (franzs@franzs-nb) (aarch64-none-linux-gnu-gcc (Arm GNU Toolchain 12.3.Rel1 (Build arm-12.35)4
[    0.000000] KASLR disabled due to lack of seed
[    0.000000] Machine model: Toradex Verdin AM62 WB on Verdin Development Board
[    0.000000] efi: UEFI not found.
[    0.000000] OF: reserved mem: 0x0000000080000000..0x000000008007ffff (512 KiB) nomap non-reusable tfa@80000000
[    0.000000] Reserved memory: created DMA memory pool at 0x000000009db00000, size 12 MiB
[    0.000000] OF: reserved mem: initialized node r5f-dma-memory@9db00000, compatible id shared-dma-pool
[    0.000000] OF: reserved mem: 0x000000009db00000..0x000000009e6fffff (12288 KiB) nomap non-reusable r5f-dma-memory@9db00000
[    0.000000] OF: reserved mem: 0x000000009e800000..0x000000009fffffff (24576 KiB) nomap non-reusable optee@9e800000
[    0.000000] Zone ranges:
[    0.000000]   DMA      [mem 0x0000000080000000-0x00000000ffffffff]
[    0.000000]   DMA32    empty
[    0.000000]   Normal   empty
[    0.000000] Movable zone start for each node
[    0.000000] Early memory node ranges
[    0.000000]   node   0: [mem 0x0000000080000000-0x000000008007ffff]
[    0.000000]   node   0: [mem 0x0000000080080000-0x000000009dafffff]
[    0.000000]   node   0: [mem 0x000000009db00000-0x000000009e6fffff]
[    0.000000]   node   0: [mem 0x000000009e700000-0x000000009e7fffff]
[    0.000000]   node   0: [mem 0x000000009e800000-0x000000009fffffff]
[    0.000000]   node   0: [mem 0x00000000a0000000-0x00000000ffffffff]
[    0.000000] Initmem setup node 0 [mem 0x0000000080000000-0x00000000ffffffff]
[    0.000000] cma: Reserved 128 MiB at 0x00000000f5a00000 on node -1
[    0.000000] psci: probing for conduit method from DT.
[    0.000000] psci: PSCIv1.1 detected in firmware.
[    0.000000] psci: Using standard PSCI v0.2 function IDs
[    0.000000] psci: Trusted OS migration not required
[    0.000000] psci: SMC Calling Convention v1.5
[    0.000000] percpu: Embedded 20 pages/cpu s43176 r8192 d30552 u81920
[    0.000000] Detected VIPT I-cache on CPU0
[    0.000000] CPU features: detected: GIC system register CPU interface
[    0.000000] CPU features: detected: ARM erratum 845719
[    0.000000] alternatives: applying boot alternatives
[    0.000000] Kernel command line: root=PARTUUID=c4e4fc06-02 ro rootwait console=tty1 console=ttyS2,115200
[    0.000000] Dentry cache hash table entries: 262144 (order: 9, 2097152 bytes, linear)
[    0.000000] Inode-cache hash table entries: 131072 (order: 8, 1048576 bytes, linear)
[    0.000000] Built 1 zonelists, mobility grouping on.  Total pages: 516096
[    0.000000] mem auto-init: stack:all(zero), heap alloc:off, heap free:off
[    0.000000] software IO TLB: area num 4.
[    0.000000] software IO TLB: mapped [mem 0x00000000f1800000-0x00000000f5800000] (64MB)
[    0.000000] Memory: 1801684K/2097152K available (11904K kernel code, 1398K rwdata, 3540K rodata, 2624K init, 491K bss, 164396K reserved, 131072K c)
[    0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=4, Nodes=1
[    0.000000] rcu: Preemptible hierarchical RCU implementation.
[    0.000000] rcu:     RCU restricting CPUs from NR_CPUS=256 to nr_cpu_ids=4.
[    0.000000]  Trampoline variant of Tasks RCU enabled.
[    0.000000]  Tracing variant of Tasks RCU enabled.
[    0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 25 jiffies.
[    0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=4
[    0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0
[    0.000000] GICv3: GIC: Using split EOI/Deactivate mode
[    0.000000] GICv3: 256 SPIs implemented
[    0.000000] GICv3: 0 Extended SPIs implemented
[    0.000000] Root IRQ handler: gic_handle_irq
[    0.000000] GICv3: GICv3 features: 16 PPIs
[    0.000000] GICv3: CPU0: found redistributor 0 region 0:0x0000000001880000
[    0.000000] ITS [mem 0x01820000-0x0182ffff]
[    0.000000] GIC: enabling workaround for ITS: Socionext Synquacer pre-ITS
[    0.000000] ITS@0x0000000001820000: Devices Table too large, reduce ids 20->19
[    0.000000] ITS@0x0000000001820000: allocated 524288 Devices @80c00000 (flat, esz 8, psz 64K, shr 0)
[    0.000000] ITS: using cache flushing for cmd queue
[    0.000000] GICv3: using LPI property table @0x0000000080440000
[    0.000000] GIC: using cache flushing for LPI property table
[    0.000000] GICv3: CPU0: using allocated LPI pending table @0x0000000080450000
[    0.000000] rcu: srcu_init: Setting srcu_struct sizes based on contention.
[    0.000000] arch_timer: cp15 timer(s) running at 200.00MHz (phys).
[    0.000000] clocksource: arch_sys_counter: mask: 0x3ffffffffffffff max_cycles: 0x2e2049d3e8, max_idle_ns: 440795210634 ns
[    0.000001] sched_clock: 58 bits at 200MHz, resolution 5ns, wraps every 4398046511102ns
[    0.000423] Console: colour dummy device 80x25
[    0.000437] printk: console [tty1] enabled
[    0.000990] Calibrating delay loop (skipped), value calculated using timer frequency.. 400.00 BogoMIPS (lpj=800000)
[    0.001016] pid_max: default: 32768 minimum: 301
[    0.001124] LSM: initializing lsm=capability,integrity
[    0.001267] Mount-cache hash table entries: 4096 (order: 3, 32768 bytes, linear)
[    0.001303] Mountpoint-cache hash table entries: 4096 (order: 3, 32768 bytes, linear)
[    0.003551] RCU Tasks: Setting shift to 2 and lim to 1 rcu_task_cb_adjust=1.
[    0.003661] RCU Tasks Trace: Setting shift to 2 and lim to 1 rcu_task_cb_adjust=1.
[    0.003958] rcu: Hierarchical SRCU implementation.
[    0.003975] rcu:     Max phase no-delay instances is 1000.
[    0.004701] Platform MSI: msi-controller@1820000 domain created
[    0.005103] PCI/MSI: /bus@f0000/interrupt-controller@1800000/msi-controller@1820000 domain created
[    0.005409] EFI services will not be available.
[    0.005829] smp: Bringing up secondary CPUs ...
[    0.006587] Detected VIPT I-cache on CPU1
[    0.006690] GICv3: CPU1: found redistributor 1 region 0:0x00000000018a0000
[    0.006709] GICv3: CPU1: using allocated LPI pending table @0x0000000080460000
[    0.006779] CPU1: Booted secondary processor 0x0000000001 [0x410fd034]
[    0.007615] Detected VIPT I-cache on CPU2
[    0.007680] GICv3: CPU2: found redistributor 2 region 0:0x00000000018c0000
[    0.007695] GICv3: CPU2: using allocated LPI pending table @0x0000000080470000
[    0.007734] CPU2: Booted secondary processor 0x0000000002 [0x410fd034]
[    0.008527] Detected VIPT I-cache on CPU3
[    0.008590] GICv3: CPU3: found redistributor 3 region 0:0x00000000018e0000
[    0.008606] GICv3: CPU3: using allocated LPI pending table @0x0000000080480000
[    0.008642] CPU3: Booted secondary processor 0x0000000003 [0x410fd034]
[    0.008736] smp: Brought up 1 node, 4 CPUs
[    0.008852] SMP: Total of 4 processors activated.
[    0.008865] CPU features: detected: 32-bit EL0 Support
[    0.008877] CPU features: detected: CRC32 instructions
[    0.008954] CPU: All CPU(s) started at EL2
[    0.008966] alternatives: applying system-wide alternatives
[    0.011132] devtmpfs: initialized
[    0.021936] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns
[    0.022008] futex hash table entries: 1024 (order: 4, 65536 bytes, linear)
[    0.027722] pinctrl core: initialized pinctrl subsystem
[    0.028518] DMI not present or invalid.
[    0.029327] NET: Registered PF_NETLINK/PF_ROUTE protocol family
[    0.030454] DMA: preallocated 256 KiB GFP_KERNEL pool for atomic allocations
[    0.030636] DMA: preallocated 256 KiB GFP_KERNEL|GFP_DMA pool for atomic allocations
[    0.030803] DMA: preallocated 256 KiB GFP_KERNEL|GFP_DMA32 pool for atomic allocations
[    0.030932] audit: initializing netlink subsys (disabled)
[    0.031226] audit: type=2000 audit(0.028:1): state=initialized audit_enabled=0 res=1
[    0.031758] thermal_sys: Registered thermal governor 'step_wise'
[    0.031764] thermal_sys: Registered thermal governor 'power_allocator'
[    0.031876] cpuidle: using governor menu
[    0.032047] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers.
[    0.032153] ASID allocator initialised with 65536 entries
[    0.047469] platform 30200000.dss: Fixed dependency cycle(s) with /bus@f0000/dss@30200000/oldi-txes/oldi@0
[    0.047543] platform 30200000.dss: Fixed dependency cycle(s) with /bus@f0000/dss@30200000/oldi-txes/oldi@1
[    0.049550] platform connector: Fixed dependency cycle(s) with /bus@f0000/dwc3-usb@f900000/usb@31000000
[    0.052021] Modules: 27744 pages in range for non-PLT usage
[    0.052036] Modules: 519264 pages in range for PLT usage
[    0.053074] HugeTLB: registered 1.00 GiB page size, pre-allocated 0 pages
[    0.053112] HugeTLB: 0 KiB vmemmap can be freed for a 1.00 GiB page
[    0.053126] HugeTLB: registered 32.0 MiB page size, pre-allocated 0 pages
[    0.053137] HugeTLB: 0 KiB vmemmap can be freed for a 32.0 MiB page
[    0.053148] HugeTLB: registered 2.00 MiB page size, pre-allocated 0 pages
[    0.053159] HugeTLB: 0 KiB vmemmap can be freed for a 2.00 MiB page
[    0.053171] HugeTLB: registered 64.0 KiB page size, pre-allocated 0 pages
[    0.053181] HugeTLB: 0 KiB vmemmap can be freed for a 64.0 KiB page
[    0.055044] k3-chipinfo 43000014.chipid: Family:AM62X rev:SR1.0 JTAGID[0x0bb7e02f] Detected
[    0.056075] iommu: Default domain type: Translated
[    0.056112] iommu: DMA domain TLB invalidation policy: strict mode
[    0.056465] SCSI subsystem initialized
[    0.056880] usbcore: registered new interface driver usbfs
[    0.056918] usbcore: registered new interface driver hub
[    0.056962] usbcore: registered new device driver usb
[    0.057612] pps_core: LinuxPPS API ver. 1 registered
[    0.057626] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[    0.057652] PTP clock support registered
[    0.057857] EDAC MC: Ver: 3.0.0
[    0.058469] scmi_core: SCMI protocol bus registered
[    0.058783] FPGA manager framework
[    0.058891] Advanced Linux Sound Architecture Driver Initialized.
[    0.060038] vgaarb: loaded
[    0.060485] clocksource: Switched to clocksource arch_sys_counter
[    0.060810] VFS: Disk quotas dquot_6.6.0
[    0.060860] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes)
[    0.067139] NET: Registered PF_INET protocol family
[    0.067466] IP idents hash table entries: 32768 (order: 6, 262144 bytes, linear)
[    0.069318] tcp_listen_portaddr_hash hash table entries: 1024 (order: 2, 16384 bytes, linear)
[    0.069387] Table-perturb hash table entries: 65536 (order: 6, 262144 bytes, linear)
[    0.069411] TCP established hash table entries: 16384 (order: 5, 131072 bytes, linear)
[    0.069587] TCP bind hash table entries: 16384 (order: 7, 524288 bytes, linear)
[    0.070310] TCP: Hash tables configured (established 16384 bind 16384)
[    0.070558] UDP hash table entries: 1024 (order: 3, 32768 bytes, linear)
[    0.070630] UDP-Lite hash table entries: 1024 (order: 3, 32768 bytes, linear)
[    0.070897] NET: Registered PF_UNIX/PF_LOCAL protocol family
[    0.071552] RPC: Registered named UNIX socket transport module.
[    0.071579] RPC: Registered udp transport module.
[    0.071589] RPC: Registered tcp transport module.
[    0.071598] RPC: Registered tcp-with-tls transport module.
[    0.071608] RPC: Registered tcp NFSv4.1 backchannel transport module.
[    0.071625] NET: Registered PF_XDP protocol family
[    0.071663] PCI: CLS 0 bytes, default 64
[    0.073362] Initialise system trusted keyrings
[    0.073699] workingset: timestamp_bits=46 max_order=19 bucket_order=0
[    0.074073] squashfs: version 4.0 (2009/01/31) Phillip Lougher
[    0.074376] NFS: Registering the id_resolver key type
[    0.074414] Key type id_resolver registered
[    0.074425] Key type id_legacy registered
[    0.074452] nfs4filelayout_init: NFSv4 File Layout Driver Registering...
[    0.074467] nfs4flexfilelayout_init: NFSv4 Flexfile Layout Driver Registering...
[    0.105691] Key type asymmetric registered
[    0.105714] Asymmetric key parser 'x509' registered
[    0.105790] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 245)
[    0.105996] io scheduler mq-deadline registered
[    0.106010] io scheduler kyber registered
[    0.106059] io scheduler bfq registered
[    0.110117] pinctrl-single 4084000.pinctrl: 34 pins, size 136
[    0.111132] pinctrl-single f4000.pinctrl: 171 pins, size 684
[    0.119398] Serial: 8250/16550 driver, 6 ports, IRQ sharing enabled
[    0.132143] brd: module loaded
[    0.137733] loop: module loaded
[    0.142863] tun: Universal TUN/TAP device driver, 1.6
[    0.144102] VFIO - User Level meta-driver version: 0.3
[    0.145199] usbcore: registered new interface driver usb-storage
[    0.145280] usbcore: registered new device driver onboard-usb-hub
[    0.146336] i2c_dev: i2c /dev entries driver
[    0.148895] sdhci: Secure Digital Host Controller Interface driver
[    0.148935] sdhci: Copyright(c) Pierre Ossman
[    0.149207] sdhci-pltfm: SDHCI platform and OF driver helper
[    0.149923] ledtrig-cpu: registered to indicate activity on CPUs
[    0.150274] SMCCC: SOC_ID: ARCH_SOC_ID not implemented, skipping ....
[    0.151006] usbcore: registered new interface driver usbhid
[    0.151021] usbhid: USB HID core driver
[    0.151431] omap-mailbox 29000000.mailbox: omap mailbox rev 0x66fc9100
[    0.153248] hw perfevents: enabled with armv8_cortex_a53 PMU driver, 7 counters available
[    0.154024] optee: probing for conduit method.
[    0.154074] optee: revision 4.2 (12d7c4ee)
[    0.154449] optee: dynamic shared memory is enabled
[    0.154905] optee: initialized driver
[    0.157270] Initializing XFRM netlink socket
[    0.157351] NET: Registered PF_PACKET protocol family
[    0.157456] Key type dns_resolver registered
[    0.165019] registered taskstats version 1
[    0.165273] Loading compiled-in X.509 certificates
[    0.179399] ti-sci 44043000.system-controller: ABI: 4.0 (firmware rev 0x000a '10.0.8--v10.00.08 (Fiery Fox)')
[    0.227780] ti-sci-clk 44043000.system-controller:clock-controller: recalc-rate failed for dev=81, clk=20, ret=-19
[    0.253284] omap_i2c 4900000.i2c: bus 3 rev0.12 at 100 kHz
[    0.254561] i2c 0-0030: Fixed dependency cycle(s) with /bus@f0000/i2c@20000000/pmic@30/regulators/buck2
[    0.279436] input: tps65219-pwrbutton as /devices/platform/bus@f0000/20000000.i2c/i2c-0/0-0030/tps65219-pwrbutton.2.auto/input/input0
[    0.281816] rtc-ds1307 0-0032: oscillator failed, set time!
[    0.282059] rtc-ds1307 0-0032: registered as rtc0
[    0.282224] rtc-ds1307 0-0032: hctosys: unable to read the hardware clock
[    0.284706] at24 0-0050: supply vcc not found, using dummy regulator
[    0.285254] at24 0-0050: 256 byte 24c02 EEPROM, writable, 16 bytes/write
[    0.285345] omap_i2c 20000000.i2c: bus 0 rev0.12 at 400 kHz
[    0.287427] pca953x 1-0021: supply vcc not found, using dummy regulator
[    0.287615] pca953x 1-0021: using no AI
[    0.308618] pca953x 1-0021: failed writing register
[    0.308799] pca953x: probe of 1-0021 failed with error -121
[    0.309447] at24 1-0057: supply vcc not found, using dummy regulator
[    0.310245] at24 1-0057: 256 byte 24c02 EEPROM, writable, 16 bytes/write
[    0.310315] omap_i2c 20010000.i2c: bus 1 rev0.12 at 100 kHz
[    0.312115] omap_i2c 20020000.i2c: bus 2 rev0.12 at 100 kHz
[    0.313525] omap_i2c 20030000.i2c: bus 4 rev0.12 at 100 kHz
[    0.313818] ti-sci-intr 4210000.interrupt-controller: Interrupt Router 5 domain created
[    0.314003] ti-sci-intr bus@f0000:interrupt-controller@a00000: Interrupt Router 3 domain created
[    0.314267] ti-sci-inta 48000000.interrupt-controller: Interrupt Aggregator domain 28 created
[    0.316389] ti-udma 485c0100.dma-controller: Number of rings: 82
[    0.319190] ti-udma 485c0100.dma-controller: Channels: 48 (bchan: 18, tchan: 12, rchan: 18)
[    0.322071] ti-udma 485c0000.dma-controller: Number of rings: 150
[    0.327274] ti-udma 485c0000.dma-controller: Channels: 35 (tchan: 20, rchan: 15)
[    0.330849] 4a00000.serial: ttyS3 at MMIO 0x4a00000 (irq = 291, base_baud = 3000000) is a 8250
[    0.332528] 2800000.serial: ttyS2 at MMIO 0x2800000 (irq = 292, base_baud = 3000000) is a 8250
[    0.332641] printk: console [ttyS2] enabled
[    1.785103] 2810000.serial: ttyS0 at MMIO 0x2810000 (irq = 293, base_baud = 3000000) is a 8250
[    1.794781] omap8250 2850000.serial: PM domain pd:156 will not be powered off
[    1.802654] 2850000.serial: ttyS4 at MMIO 0x2850000 (irq = 294, base_baud = 3000000) is a 8250
[    1.811469] serial serial0: tty port ttyS4 registered
[    1.820004] davinci_mdio 8000f00.mdio: Configuring MDIO in manual mode
[    1.864489] davinci_mdio 8000f00.mdio: davinci mdio revision 9.7, bus freq 1000000
[    1.873553] am65-cpsw-nuss 8000000.ethernet: initializing am65 cpsw nuss version 0x6BA01103, cpsw version 0x6BA81103 Ports: 3 quirks:00000006
[    1.886528] am65-cpsw-nuss 8000000.ethernet: initialized cpsw ale version 1.5
[    1.893672] am65-cpsw-nuss 8000000.ethernet: ALE Table size 512
[    1.900496] am65-cpsw-nuss 8000000.ethernet: CPTS ver 0x4e8a010c, freq:500000000, add_val:1 pps:0
[    1.916141] am65-cpsw-nuss 8000000.ethernet: set new flow-id-base 19
[    1.927377] platform connector: Fixed dependency cycle(s) with /bus@f0000/dwc3-usb@f900000/usb@31000000
[    1.936973] platform 31000000.usb: Fixed dependency cycle(s) with /connector
[    1.949699] xhci-hcd xhci-hcd.3.auto: xHCI Host Controller
[    1.955285] xhci-hcd xhci-hcd.3.auto: new USB bus registered, assigned bus number 1
[    1.963095] xhci-hcd xhci-hcd.3.auto: USB3 root hub has no ports
[    1.969109] xhci-hcd xhci-hcd.3.auto: hcc params 0x0258fe6d hci version 0x110 quirks 0x0000008000000010
[    1.978571] xhci-hcd xhci-hcd.3.auto: irq 308, io mem 0x31100000
[    1.985520] hub 1-0:1.0: USB hub found
[    1.989372] hub 1-0:1.0: 1 port detected
[    2.002275] mmc0: CQHCI version 5.10
[    2.013074] davinci_mdio 8000f00.mdio: Configuring MDIO in manual mode
[    2.044501] mmc0: SDHCI controller on fa10000.mmc [fa10000.mmc] using ADMA 64-bit
[    2.056503] davinci_mdio 8000f00.mdio: davinci mdio revision 9.7, bus freq 1000000
[    2.071093] mdio_bus 8000f00.mdio: MDIO device at address 7 is missing.
[    2.077755] davinci_mdio 8000f00.mdio: phy[0]: device 8000f00.mdio:00, driver TI DP83867
[    2.089401] sdhci-am654 fa00000.mmc: Got CD GPIO
[    2.089401] sdhci-am654 fa20000.mmc: allocated mmc-pwrseq
[    2.089992] mmc1: CQHCI version 5.10
[    2.093182] input: gpio-keys as /devices/platform/gpio-keys/input/input1
[    2.094189] clk: Disabling unused clocks
[    2.099891] mmc2: CQHCI version 5.10
[    2.107599] ti-sci-clk 44043000.system-controller:clock-controller: is_prepared failed for dev=81, clk=20, ret=-19
[    2.132980] ALSA device list:
[    2.135965]   No soundcards found.
[    2.148505] mmc2: SDHCI controller on fa20000.mmc [fa20000.mmc] using ADMA 64-bit
[    2.151403] mmc1: SDHCI controller on fa00000.mmc [fa00000.mmc] using ADMA 64-bit
[    2.164174] Waiting for root device PARTUUID=c4e4fc06-02...
[    2.185518] mmc0: Command Queue Engine enabled
[    2.190019] mmc0: new HS200 MMC card at address 0001
[    2.195895] mmcblk0: mmc0:0001 S40016 14.6 GiB
[    2.200637] mmc2: new ultra high speed DDR50 SDIO card at address 0001
[    2.202359]  mmcblk0: p1 p2
[    2.210795] mmcblk0boot0: mmc0:0001 S40016 4.00 MiB
[    2.217020] mmcblk0boot1: mmc0:0001 S40016 4.00 MiB
[    2.223024] mmcblk0rpmb: mmc0:0001 S40016 4.00 MiB, chardev (241:0)
[    2.241333] EXT4-fs (mmcblk0p2): mounted filesystem 39ce6525-0e37-4270-952f-47a700c53e22 ro with ordered data mode. Quota mode: none.
[    2.253595] VFS: Mounted root (ext4 filesystem) readonly on device 179:2.
[    2.256528] usb 1-1: new high-speed USB device number 2 using xhci-hcd
[    2.263764] devtmpfs: mounted
[    2.271714] Freeing unused kernel memory: 2624K
[    2.276498] Run /sbin/init as init process
[    2.417860] systemd[1]: System time before build time, advancing clock.
[    2.440128] systemd[1]: Failed to find module 'autofs4'
[    2.464453] NET: Registered PF_INET6 protocol family
[    2.465214] hub 1-1:1.0: USB hub found
[    2.471264] Segment Routing with IPv6
[    2.473420] hub 1-1:1.0: 4 ports detected
[    2.477036] In-situ OAM (IOAM) with IPv6
[    2.511700] systemd[1]: systemd 255.4^ running in system mode (+PAM -AUDIT -SELINUX -APPARMOR +IMA -SMACK +SECCOMP -GCRYPT -GNUTLS -OPENSSL +ACL +)
[    2.543710] systemd[1]: Detected architecture arm64.

Welcome to TDX Wayland with XWayland 7.0.0-devel-20240904+build.120 (scarthgap)!

[    2.570298] systemd[1]: Hostname set to <verdin-am62-15412844>.
[    2.625281] hub 1-1:1.0: USB hub found
[    2.629555] hub 1-1:1.0: 4 ports detected
[    2.976546] usb 1-1.4: new high-speed USB device number 3 using xhci-hcd
[    3.040325] systemd[1]: Queued start job for default target Graphical Interface.
[    3.083542] omap8250 2b300000.serial: No clock speed specified: using default: 48000000
[    3.092807] 2b300000.serial: ttyS1 at MMIO 0x2b300000 (irq = 493, base_baud = 3000000) is a 8250
[    3.099659] systemd[1]: Created slice Slice /system/getty.
[  OK  ] Created slice Slice /system/getty.
[    3.127694] systemd[1]: Created slice Slice /system/modprobe.
[  OK  ] Created slice Slice /system/modprobe.
[    3.151641] systemd[1]: Created slice Slice /system/serial-getty.
[  OK  ] Created slice Slice /system/serial-getty.
[    3.175296] systemd[1]: Created slice User and Session Slice.
[  OK  ] Created slice User and Session Slice.
[    3.197427] systemd[1]: Started Dispatch Password Requests to Console Directory Watch.
[  OK  ] Started Dispatch Password Requests to Console Directory Watch.
[    3.221469] systemd[1]: Started Forward Password Requests to Wall Directory Watch.
[  OK  ] Started Forward Password Requests to Wall Directory Watch.
[    3.244961] systemd[1]: Expecting device /dev/ttyS2...
         Expecting device /dev/ttyS2...
[    3.261088] systemd[1]: Reached target Host and Network Name Lookups.
[  OK  ] Reached target Host and Network Name Lookups.
[    3.284890] systemd[1]: Reached target Path Units.
[  OK  ] Reached target Path Units.
[    3.300876] systemd[1]: Reached target Remote File Systems.
[  OK  ] Reached target Remote File Systems.
[    3.321131] systemd[1]: Reached target Slice Units.
[  OK  ] Reached target Slice Units.
[    3.337097] systemd[1]: Reached target Swaps.
[  OK  ] Reached target Swaps.
[    3.431232] systemd[1]: Listening on RPCbind Server Activation Socket.
[  OK  ] Listening on RPCbind Server Activation Socket.
[    3.453193] systemd[1]: Reached target RPC Port Mapper.
[  OK  ] Reached target RPC Port Mapper.
[    3.480072] systemd[1]: Listening on Syslog Socket.
[  OK  ] Listening on Syslog Socket.
[    3.497925] systemd[1]: Listening on initctl Compatibility Named Pipe.
[  OK  ] Listening on initctl Compatibility Named Pipe.
[    3.525949] systemd[1]: Listening on Journal Audit Socket.
[  OK  ] Listening on Journal Audit Socket.
[    3.551635] systemd[1]: Listening on Journal Socket (/dev/log).
[  OK  ] Listening on Journal Socket (/dev/log).
[    3.576285] systemd[1]: Listening on Journal Socket.
[  OK  ] Listening on Journal Socket.
[    3.600830] systemd[1]: Listening on Network Service Netlink Socket.
[  OK  ] Listening on Network Service Netlink Socket.
[    3.632662] systemd[1]: Listening on udev Control Socket.
[  OK  ] Listening on udev Control Socket.
[    3.655581] systemd[1]: Listening on udev Kernel Socket.
[  OK  ] Listening on udev Kernel Socket.
[    3.679712] systemd[1]: Listening on User Database Manager Socket.
[  OK  ] Listening on User Database Manager Socket.
[    3.745078] systemd[1]: Mounting Huge Pages File System...
         Mounting Huge Pages File System...
[    3.770070] systemd[1]: Mounting POSIX Message Queue File System...
         Mounting POSIX Message Queue File System...
[    3.798052] systemd[1]: Mounting Kernel Debug File System...
         Mounting Kernel Debug File System...
[    3.817819] systemd[1]: Kernel Trace File System was skipped because of an unmet condition check (ConditionPathExists=/sys/kernel/tracing).
[    3.837686] systemd[1]: Mounting Temporary Directory /tmp...
         Mounting Temporary Directory /tmp...
[    3.868185] systemd[1]: Starting Create List of Static Device Nodes...
         Starting Create List of Static Device Nodes...
[    3.899783] systemd[1]: Starting Load Kernel Module configfs...
         Starting Load Kernel Module configfs...
[    3.927574] systemd[1]: Starting Load Kernel Module drm...
         Starting Load Kernel Module drm...
[    3.955522] systemd[1]: Starting Load Kernel Module fuse...
         Starting Load Kernel Module fuse...
[    3.985513] systemd[1]: Starting RPC Bind...
         Starting RPC Bind...
[    4.000081] fuse: init (API version 7.39)
[    4.011132] systemd[1]: Starting File System Check on Root Device...
         Starting File System Check on Root Device...
[    4.071069] systemd[1]: Starting Journal Service...
         Starting Journal Service...
[    4.095454] systemd[1]: Load Kernel Modules was skipped because no trigger condition checks were met.
[    4.129679] systemd[1]: Starting Generate network units from Kernel command line...
         Starting Generate network units from Kernel command line...
[    4.145168] systemd[1]: Starting Apply Kernel Variables...
         Starting Apply Kernel Variables...
[    4.166102] systemd[1]: Starting Coldplug All udev Devices...
         Starting Coldplug All udev Devices...
[    4.199624] systemd[1]: Started RPC Bind.
[  OK  ] Started RPC Bind.
[    4.222291] systemd[1]: Mounted Huge Pages File System.
[    4.225852] systemd-journald[131]: Collecting audit messages is enabled.
[  OK  ] Mounted Huge Pages File System.
[    4.258653] systemd[1]: Mounted POSIX Message Queue File System.
[  OK  ] Mounted POSIX Message Queue File System.
[    4.281951] systemd[1]: Mounted Kernel Debug File System.
[  OK  ] Mounted Kernel Debug File System.
[    4.305991] systemd[1]: Mounted Temporary Directory /tmp.
[  OK  ] Mounted Temporary Directory /tmp.
[    4.333613] systemd[1]: Started Journal Service.
[  OK  ] Started Journal Service.
[  OK  ] Finished Create List of Static Device Nodes.
[  OK  ] Finished Load Kernel Module configfs.
[  OK  ] Finished Load Kernel Module drm.
[  OK  ] Finished Load Kernel Module fuse.
[  OK  ] Finished File System Check on Root Device.
[  OK  ] Finished Generate network units from Kernel command line.
[  OK  ] Finished Apply Kernel Variables.
         Mounting FUSE Control File System...
         Mounting Kernel Configuration File System...
         Starting Remount Root and Kernel File Systems...
         Starting Create Static Device Nodes in /dev gracefully...
[  OK  ] Mounted FUSE Control File System.
[  OK  ] Mounted Kernel Configuration File System.
[    4.734010] EXT4-fs (mmcblk0p2): re-mounted 39ce6525-0e37-4270-952f-47a700c53e22 r/w. Quota mode: none.
[  OK  ] Finished Remount Root and Kernel File Systems.
[  OK  ] Finished Create Static Device Nodes in /dev gracefully.
         Starting Flush Journal to Persistent Storage...
         Starting Create Static Device Nodes in /dev...
[    4.867643] systemd-journald[131]: Received client request to flush runtime journal.
[  OK  ] Finished Flush Journal to Persistent Storage.
[  OK  ] Finished Create Static Device Nodes in /dev.
[  OK  ] Reached target Preparation for Local File Systems.
[    4.960407] audit: type=1334 audit(1709054766.536:2): prog-id=6 op=LOAD
[    4.967187] audit: type=1334 audit(1709054766.544:3): prog-id=7 op=LOAD
         Starting Rule-based Manager for Device Events and Files...
[  OK  ] Finished Coldplug All udev Devices.
[  OK  ] Started Rule-based Manager for Device Events and Files.
         Mounting /var/volatile...
[  OK  ] Mounted /var/volatile.
         Starting Load/Save OS Random Seed...
[  OK  ] Reached target Local File Systems.
         Starting Create Volatile Files and Directories...
[  OK  ] Finished Create Volatile Files and Directories.
[    5.618593] audit: type=1334 audit(1709054767.192:4): prog-id=8 op=LOAD
         Starting Network Time Synchronization...
         Starting Record System Boot/Shutdown in UTMP...
[    5.872634] audit: type=1334 audit(1709054767.448:5): prog-id=9 op=LOAD
[    5.886510] audit: type=1334 audit(1709054767.448:6): prog-id=10 op=LOAD
[    5.900643] audit: type=1334 audit(1709054767.448:7): prog-id=11 op=LOAD
         Starting User Database Manager...
[  OK  ] Finished Record System Boot/Shutdown in UTMP.
[  OK  ] Started User Database Manager.
[  OK  ] Found device /dev/ttyS2.
[    6.324595] random: crng init done
[  OK  ] Finished Load/Save OS Random Seed.
[  OK  ] Started Network Time Synchronization.
[  OK  ] Reached target System Initialization.
[  OK  ] Started Daily Cleanup of Temporary Directories.
[  OK  ] Reached target System Time Set.
[  OK  ] Reached target Timer Units.
[  OK  ] Listening on Avahi mDNS/DNS-SD Stack Activation Socket.
[  OK  ] Listening on D-Bus System Message Bus Socket.
[  OK  ] Listening on dropbear.socket.
[  OK  ] Listening on GPS (Global Positioning System) Daemon Sockets.
         Starting Weston socket...
[    6.903138] lm75 0-0048: supply vs not found, using dummy regulator
[    6.915536] hwmon hwmon1: temp1_input not attached to any thermal zone
[    6.925325] lm75 0-0048: hwmon1: sensor 'tmp1075'
[    6.935111] lm75 1-004f: supply vs not found, using dummy regulator

[    6.947001] CAN device driver interface
[    6.953404] hwmon hwmon2: temp1_input not attached to any thermal zone
[  OK  ] Reached target Socket Units.
[    6.961311] nau8822 1-001a: Failed to issue reset: -121
[    6.965511] lm75 1-004f: hwmon2: sensor 'tmp75c'
[    6.975714] nau8822: probe of 1-001a failed with error -121
[  OK  ] Reached target Basic System.
[    6.983792] atmel_mxt_ts 2-004a: supply vdda not found, using dummy regulator
[    6.999181] ina2xx 1-0040: supply vs not found, using dummy regulator
[    7.008340] ina2xx 1-0040: error configuring the device: -121
[    7.012175] atmel_mxt_ts 2-004a: supply vdd not found, using dummy regulator
[  OK  ] Started Kernel Logging Service.
[  OK  ] Started System Logging Service.[    7.067787] m_can_platform 4e08000.can: m_can device registered (irq=0, version=32)

[    7.101375] tidss 30200000.dss: failed to init OLDI: -517
[    7.111595] m_can_platform 20701000.can: m_can device registered (irq=498, version=32)
[    7.122254] tidss 30200000.dss: failed to init OLDI: -517
         Starting D-Bus System Message Bus...
         Starting IPv6 Packet Filtering Framework...
         Starting IPv4 Packet Filtering Framework..[    7.203355] tidss 30200000.dss: failed to init OLDI: -517
.
[    7.234866] tidss 30200000.dss: failed to init OLDI: -517
         Starting Telephony service...
[    7.276199] Bluetooth: Core ver 2.22
[    7.293660] rtc-ti-k3 2b1f0000.rtc: registered as rtc1
[    7.299057] tidss 30200000.dss: failed to init OLDI: -517
[    7.305294] NET: Registered PF_BLUETOOTH protocol family
[    7.305393] audit: type=1334 audit(1725613782.929:8): prog-id=12 op=LOAD
[    7.310718] atmel_mxt_ts 2-004a: Family: 164 Variant: 11 Firmware V1.2.AA Objects: 41
[    7.310937] Bluetooth: HCI device and connection manager initialized
[    7.310969] Bluetooth: HCI socket layer initialized
[    7.310980] Bluetooth: L2CAP socket layer initialized
[    7.311041] Bluetooth: SCO socket layer initialized
[    7.318867] tidss 30200000.dss: failed to init OLDI: -517
[    7.326987] audit: type=1334 audit(1725613782.949:9): prog-id=13 op=LOAD
[    7.343035] atmel_mxt_ts 2-004a: Enabling RETRIGEN workaround
[    7.350820] audit: type=1334 audit(1725613782.953:10): prog-id=14 op=LOAD
         Starting User Login Management...
[    7.394062] platform 78000000.r5f: R5F core may have been powered on by a different host, programmed state (0) != actual state (1)
[  OK  ] Started Timestamping service.
[  OK  ] Started D-Bus System Message Bus.
[    7.488902] atmel_mxt_ts 2-004a: Direct firmware load for maxtouch.cfg failed with error -2
[  OK  ] Finished IPv6 Packet Filtering Fram[    7.501677] tidss 30200000.dss: failed to init OLDI: -517
ework.
[    7.507650] platform 78000000.r5f: configured R5F for IPC-only mode
[  OK  ] Finished IPv4 Packet Filtering Fram[    7.526383] platform 78000000.r5f: device does not have reserved memory regions, ret = -22
ework.
[    7.540384] k3_r5_rproc bus@f0000:bus@b00000:r5fss@78000000: reserved memory init failed, ret = -22
[    7.551540] atmel_mxt_ts 2-004a: Touchscreen size X1279Y799
[    7.559547] input: Atmel maXTouch Touchscreen as /devices/platform/bus@f0000/20020000.i2c/i2c-2/2-004a/input/input2
[    7.579622] remoteproc remoteproc0: releasing 78000000.r5f
[  OK  ] Reached target Preparation for Netw[    7.595600] k3_r5_rproc bus@f0000:bus@b00000:r5fss@78000000: k3_r5_cluster_rproc_init failed, ret = -22
ork.
[    7.625118] k3_r5_rproc: probe of bus@f0000:bus@b00000:r5fss@78000000 failed with error -22
[    7.663886] cfg80211: Loading compiled-in X.509 certificates for regulatory database

[    7.682658] audit: type=1334 audit(1725613783.305:11): prog-id=15 op=LOAD
         Starting Network Configuration...
[    7.714157] Loaded X.509 cert 'sforshee: 00b28ddf47aef9cea7'
[    7.723179] Loaded X.509 cert 'wens: 61c038651aabdcf94bd0ac7ff06c7248db18c600'
[    7.786600] [drm] Initialized tidss 1.0.0 20180215 for 30200000.dss on minor 0
[    7.823145] Console: switching to colour frame buffer device 160x50
[    7.882948] tidss 30200000.dss: [drm] fb0: tidssdrmfb frame buffer device
[  OK  ] Started Telephony service.
[  OK  ] Created slice Slice /system/systemd-fsck.
         Expecting device /dev/mmcblk0p1...
         Starting Load USB gadget schemas...
[  OK  ] Started User Login Management.
[  OK  ] Started Connection service.
         Starting Avahi mDNS/DNS-SD Stack...
[    8.219863] am65-cpsw-nuss 8000000.ethernet eth0: PHY [8000f00.mdio:00] driver [TI DP83867] (irq=368)
[    8.256202] am65-cpsw-nuss 8000000.ethernet eth0: configuring for phy/rgmii-rxid link mode
[    8.309875] audit: type=1334 audit(1725613783.925:12): prog-id=16 op=LOAD
[    8.324664] audit: type=1334 audit(1725613783.929:13): prog-id=17 op=LOAD
         Starting Hostname Service...
         Starting WPA supplicant...
[  OK  ] Started Network Configuration.
[FAILED] Failed to start Load USB gadget schemas.
See 'systemctl status usbgx.service' for details.
[    8.534367] mwifiex_sdio mmc2:0001:1: info: FW download over, size 578116 bytes
[  OK  ] Created slice Slice /system/systemd-backlight.
[  OK  ] Reached target Hardware activated USB gadget.
[  OK  ] Listening on Load/Save RF Kill Switch Status /dev/rfkill Watch.
[    8.662215] remoteproc remoteproc0: 30074000.pru is available
         Starting Load/Save Screen Backligh… backlight:backlight-lvds-native...
[  OK  ] Started Avahi mDNS/DNS-SD Stack[    8.765502] remoteproc remoteproc1: 30078000.pru is available
.
[  OK  ] Started WPA supplicant.
[  OK  ] Finished Load/Save Screen Backligh…of backlight:backlight-lvds-native.
[  OK  ] Found device /dev/mmcblk0p1.
[  OK  ] Reached target Network.
         Starting File System Check on /dev/mmcblk0p1...
         Starting Permit User Sessions...
         Starting Virtual Console Setup...
[  OK  ] Started Hostname Service.
         Starting Load/Save RF Kill Switch Status...
[  OK  ] Finished Permit User Sessions.
         Starting Bluetooth service...
[  OK  ] Started Getty on tty1.
[  OK  ] Started Serial Getty on ttyS2.
[  OK  ] Reached target Login Prompts.
[  OK  ] Reached target Multi-User System.
         Starting Weston, a Wayland compositor, as a system service...
[  OK  ] Started Load/Save RF Kill Switch Status.
[  OK  ] Finished File System Check on /dev/mmcblk0p1.
[  OK  ] Finished Virtual Console Setup.
         Mounting /run/media/BOOT-mmcblk0p1...
[  OK  ] Started Bluetooth service.
         Starting BlueALSA service...
[  OK  ] Mounted /run/media/BOOT-mmcblk0p1.
[  OK  ] Created slice User Slice of UID 0.
         Mounting /boot...
         Starting User Runtime Directory /run/user/0...
[  OK  ] Mounted /boot.
[  OK  ] Started BlueALSA service.
[  OK  ] Reached target Bluetooth Support.
[  OK  ] Finished User Runtime Directory /run/user/0.
         Starting User Manager for UID 0...
[   10.060630] mwifiex_sdio mmc2:0001:1: WLAN FW is active
[   10.092743] mwifiex_sdio mmc2:0001:1: event: unknown event id: 0x81
[   10.099250] mwifiex_sdio mmc2:0001:1: Unknown GET_HW_SPEC TLV type: 0x23e
[   10.133905] mwifiex_sdio mmc2:0001:1: info: MWIFIEX VERSION: mwifiex 1.0 (16.92.21.p119) 
[   10.148175] mwifiex_sdio mmc2:0001:1: driver_version = mwifiex 1.0 (16.92.21.p119) 
[   10.369345] Bluetooth: hci0: Setting wake-up method failed (-22)
[   10.369944] Bluetooth: MGMT ver 1.22
[   10.390453] NET: Registered PF_ALG protocol family
[   10.421443] Bluetooth: RFCOMM socket layer initialized
[   10.426788] Bluetooth: RFCOMM ver 1.11
[  OK  ] Started User Manager for UID 0.
[  OK  ] Started Session c1 of User root.
[   10.762159] kauditd_printk_skb: 19 callbacks suppressed
[   10.762193] audit: type=1006 audit(1725613786.385:23): pid=577 uid=0 old-auid=4294967295 auid=0 tty=tty7 old-ses=4294967295 ses=2 res=1
[   10.780266] audit: type=1300 audit(1725613786.385:23): arch=c00000b7 syscall=64 success=yes exit=1 a0=8 a1=ffffe574c530 a2=1 a3=1 items=0 ppid=1 p)
[   10.807241] audit: type=1327 audit(1725613786.385:23): proctitle="(udevadm)"
[  OK  ] Started Session c2 of User root.
[   10.927618] audit: type=1006 audit(1725613786.549:24): pid=620 uid=0 old-auid=4294967295 auid=0 tty=tty7 old-ses=4294967295 ses=3 res=1
[   10.940252] audit: type=1300 audit(1725613786.549:24): arch=c00000b7 syscall=64 success=yes exit=1 a0=8 a1=ffffffd5b760 a2=1 a3=1 items=0 ppid=1 p)
[   10.973375] audit: type=1327 audit(1725613786.549:24): proctitle="(sh)"
[  OK  ] Started Session c3 of User root.
[   11.086391] audit: type=1006 audit(1725613786.709:25): pid=624 uid=0 old-auid=4294967295 auid=0 tty=tty7 old-ses=4294967295 ses=4 res=1
[   11.102433] audit: type=1300 audit(1725613786.709:25): arch=c00000b7 syscall=64 success=yes exit=1 a0=8 a1=ffffd6b0c490 a2=1 a3=1 items=0 ppid=1 p)
[   11.138598] audit: type=1327 audit(1725613786.709:25): proctitle="(weston)"
[   11.728649] weston[624]: memfd_create() called without MFD_EXEC or MFD_NOEXEC_SEAL set
[  OK  ] Started Weston, a Wayland compositor, as a system service.
[  OK  ] Started Start a wayland application.
[  OK  ] Reached target Graphical Interface.
         Starting Record Runlevel Change in UTMP...
[  OK  ] Started Session c4 of User root.
[  OK  ] Finished Record Runlevel Change in UTMP.
[   12.380614] Bluetooth: hci0: command tx timeout

TDX Wayland with XWayland 7.0.0-devel-20240904+build.120 (scarthgap) verdin-am62-15412844 ttyS2
Verdin-AM62_Reference-Multimedia-Image

verdin-am62-15412844 login: 
verdin-am62-15412844 login: 
verdin-am62-15412844 login: 
verdin-am62-15412844 login: root
root@verdin-am62-15412844:~# 
root@verdin-am62-15412844:~# 
root@verdin-am62-15412844:~# 
root@verdin-am62-15412844:~# [   19.166080] platform sound: deferred probe pending
[   39.645007] audit: type=1334 audit(1725613815.269:26): prog-id=18 op=UNLOAD
[   39.652103] audit: type=1334 audit(1725613815.269:27): prog-id=17 op=UNLOAD
[   39.659106] audit: type=1334 audit(1725613815.269:28): prog-id=16 op=UNLOAD

root@verdin-am62-15412844:~# 
root@verdin-am62-15412844:~# 
root@verdin-am62-15412844:~# rtcwake -s 10 -m mem -d rtc1
rtcwake: assuming RTC uses UTC ...
rtcwake: wakeup from "mem" using rtc1 at Thu Jan  1 00:02:13 1970
[  116.385983] PM: suspend entry (deep)
[  116.390061] Filesystems sync: 0.000 seconds
[  116.399417] Freezing user space processes
[  116.405492] Freezing user space processes completed (elapsed 0.001 seconds)
[  116.412567] OOM killer disabled.
[  116.415799] Freezing remaining freezable tasks
[  116.422052] Freezing remaining freezable tasks completed (elapsed 0.001 seconds)
[  116.429491] printk: Suspending console(s) (use no_console_suspend to debug)
[  116.455280] ti-sci 44043000.system-controller: ti_sci_cmd_set_device_constraint: device: 179: state: 1: ret 0
[  116.455470] ti-sci 44043000.system-controller: ti_sci_cmd_set_device_constraint: device: 178: state: 1: ret 0
[  116.465637] ti-sci 44043000.system-controller: ti_sci_cmd_set_device_constraint: device: 117: state: 1: ret 0
[  116.474162] ti-sci 44043000.system-controller: ti_sci_suspend_noirq: Saving gpio ctx dir = |5f9dffff| out = |80600000|
[  116.474925] Disabling non-boot CPUs ...
[  116.477482] psci: CPU1 killed (polled 4 ms)
[  116.482061] psci: CPU2 killed (polled 0 ms)
[  116.485581] psci: CPU3 killed (polled 0 ms)
[  116.486736] Enabling non-boot CPUs ...
[  116.487197] Detected VIPT I-cache on CPU1
[  116.487258] GICv3: CPU1: found redistributor 1 region 0:0x00000000018a0000
[  116.487330] CPU1: Booted secondary processor 0x0000000001 [0x410fd034]
[  116.488743] CPU1 is up
[  116.489032] Detected VIPT I-cache on CPU2
[  116.489064] GICv3: CPU2: found redistributor 2 region 0:0x00000000018c0000
[  116.489112] CPU2: Booted secondary processor 0x0000000002 [0x410fd034]
[  116.490174] CPU2 is up
[  116.490473] Detected VIPT I-cache on CPU3
[  116.490509] GICv3: CPU3: found redistributor 3 region 0:0x00000000018e0000
[  116.490557] CPU3: Booted secondary processor 0x0000000003 [0x410fd034]
[  116.491671] CPU3 is up
[  116.492183] ti-sci 44043000.system-controller: ti_sci_resume: restoring gpio ctx dir = |5f9dffff| out = |80600000|
[  116.492295] ti-sci 44043000.system-controller: ti_sci_resume: wakeup source: 0x50
[  116.509428] am65-cpsw-nuss 8000000.ethernet: set new flow-id-base 19
[  116.520349] am65-cpsw-nuss 8000000.ethernet eth0: PHY [8000f00.mdio:00] driver [TI DP83867] (irq=368)
[  116.521026] am65-cpsw-nuss 8000000.ethernet eth0: configuring for phy/rgmii-rxid link mode
[  116.522310] usb-conn-gpio connector: repeated role: device
[  116.785591] OOM killer enabled.
[  116.788740] Restarting tasks ... done.
[  116.794675] random: crng reseeded on system resumption
[  116.800716] PM: suspend exit
root@verdin-am62-15412844:~# 
root@verdin-am62-15412844:~# 
root@verdin-am62-15412844:~# 
root@verdin-am62-15412844:~# rtcwake -s 10 -m mem -d rtc1
rtcwake: assuming RTC uses UTC ...
rtcwake: wakeup from "mem" using rtc1 at Thu Jan  1 00:02:31 1970
[  123.714078] PM: suspend entry (deep)
[  123.718111] Filesystems sync: 0.000 seconds
[  123.723628] Freezing user space processes
[  123.729850] Freezing user space processes completed (elapsed 0.002 seconds)
[  123.736915] OOM killer disabled.
[  123.740142] Freezing remaining freezable tasks
[  123.746236] Freezing remaining freezable tasks completed (elapsed 0.001 seconds)
[  123.753658] printk: Suspending console(s) (use no_console_suspend to debug)
[  123.777801] ti-sci 44043000.system-controller: ti_sci_cmd_set_device_constraint: device: 179: state: 1: ret 0
[  123.777995] ti-sci 44043000.system-controller: ti_sci_cmd_set_device_constraint: device: 178: state: 1: ret 0
[  123.789554] ti-sci 44043000.system-controller: ti_sci_cmd_set_device_constraint: device: 117: state: 1: ret 0
[  123.798099] ti-sci 44043000.system-controller: ti_sci_suspend_noirq: Saving gpio ctx dir = |5f9dffff| out = |80600000|
[  123.798865] Disabling non-boot CPUs ...
[  123.800494] psci: CPU1 killed (polled 0 ms)
[  123.804064] psci: CPU2 killed (polled 0 ms)
[  123.807382] psci: CPU3 killed (polled 0 ms)
[  123.808842] Enabling non-boot CPUs ...
[  123.809306] Detected VIPT I-cache on CPU1
[  123.809373] GICv3: CPU1: found redistributor 1 region 0:0x00000000018a0000
[  123.809446] CPU1: Booted secondary processor 0x0000000001 [0x410fd034]
[  123.810841] CPU1 is up
[  123.811128] Detected VIPT I-cache on CPU2
[  123.811161] GICv3: CPU2: found redistributor 2 region 0:0x00000000018c0000
[  123.811205] CPU2: Booted secondary processor 0x0000000002 [0x410fd034]
[  123.812235] CPU2 is up
[  123.812527] Detected VIPT I-cache on CPU3
[  123.812564] GICv3: CPU3: found redistributor 3 region 0:0x00000000018e0000
[  123.812615] CPU3: Booted secondary processor 0x0000000003 [0x410fd034]
[  123.813766] CPU3 is up
[  123.814279] ti-sci 44043000.system-controller: ti_sci_resume: restoring gpio ctx dir = |5f9dffff| out = |80600000|
[  123.814391] ti-sci 44043000.system-controller: ti_sci_resume: wakeup source: 0x50
[  123.831312] am65-cpsw-nuss 8000000.ethernet: set new flow-id-base 19
[  123.842181] am65-cpsw-nuss 8000000.ethernet eth0: PHY [8000f00.mdio:00] driver [TI DP83867] (irq=368)
[  123.842826] am65-cpsw-nuss 8000000.ethernet eth0: configuring for phy/rgmii-rxid link mode
[  123.844126] usb-conn-gpio connector: repeated role: device
[  124.105318] OOM killer enabled.
[  124.108480] Restarting tasks ... done.
[  124.113899] random: crng reseeded on system resumption
[  124.119203] PM: suspend exit
root@verdin-am62-15412844:~# 
root@verdin-am62-15412844:~# 
root@verdin-am62-15412844:~# rtcwake -s 10 -m mem -d rtc1
rtcwake: assuming RTC uses UTC ...
rtcwake: wakeup from "mem" using rtc1 at Thu Jan  1 00:02:43 1970
[  125.728962] PM: suspend entry (deep)
[  125.733075] Filesystems sync: 0.000 seconds
[  125.738562] Freezing user space processes
[  125.744590] Freezing user space processes completed (elapsed 0.001 seconds)
[  125.751647] OOM killer disabled.
[  125.754930] Freezing remaining freezable tasks
[  125.761095] Freezing remaining freezable tasks completed (elapsed 0.001 seconds)
[  125.768547] printk: Suspending console(s) (use no_console_suspend to debug)
[  125.795475] ti-sci 44043000.system-controller: ti_sci_cmd_set_device_constraint: device: 179: state: 1: ret 0
[  125.795675] ti-sci 44043000.system-controller: ti_sci_cmd_set_device_constraint: device: 178: state: 1: ret 0
[  125.817481] ti-sci 44043000.system-controller: ti_sci_cmd_set_device_constraint: device: 117: state: 1: ret 0
[  125.826197] ti-sci 44043000.system-controller: ti_sci_suspend_noirq: Saving gpio ctx dir = |5f9dffff| out = |80600000|
[  125.826948] Disabling non-boot CPUs ...
[  125.829599] psci: CPU1 killed (polled 0 ms)
[  125.832966] psci: CPU2 killed (polled 4 ms)
[  125.836382] psci: CPU3 killed (polled 4 ms)
[  125.837239] Enabling non-boot CPUs ...
[  125.837696] Detected VIPT I-cache on CPU1
[  125.837758] GICv3: CPU1: found redistributor 1 region 0:0x00000000018a0000
[  125.837831] CPU1: Booted secondary processor 0x0000000001 [0x410fd034]
[  125.839216] CPU1 is up
[  125.839500] Detected VIPT I-cache on CPU2
[  125.839531] GICv3: CPU2: found redistributor 2 region 0:0x00000000018c0000
[  125.839573] CPU2: Booted secondary processor 0x0000000002 [0x410fd034]
[  125.840658] CPU2 is up
[  125.840961] Detected VIPT I-cache on CPU3
[  125.840997] GICv3: CPU3: found redistributor 3 region 0:0x00000000018e0000
[  125.841050] CPU3: Booted secondary processor 0x0000000003 [0x410fd034]
[  125.842204] CPU3 is up
[  125.842712] ti-sci 44043000.system-controller: ti_sci_resume: restoring gpio ctx dir = |5f9dffff| out = |80600000|
[  125.842827] ti-sci 44043000.system-controller: ti_sci_resume: wakeup source: 0x50
[  125.859546] am65-cpsw-nuss 8000000.ethernet: set new flow-id-base 19
[  125.870416] am65-cpsw-nuss 8000000.ethernet eth0: PHY [8000f00.mdio:00] driver [TI DP83867] (irq=368)
[  125.871052] am65-cpsw-nuss 8000000.ethernet eth0: configuring for phy/rgmii-rxid link mode
[  125.872378] usb-conn-gpio connector: repeated role: device
[  126.133110] OOM killer enabled.
[  126.136258] Restarting tasks ... done.
[  126.142190] random: crng reseeded on system resumption
[  126.147612] PM: suspend exit
root@verdin-am62-15412844:~# rtcwake -s 10 -m mem -d rtc1
rtcwake: assuming RTC uses UTC ...
rtcwake: wakeup from "mem" using rtc1 at Thu Jan  1 00:14:02 1970
[  794.257748] PM: suspend entry (deep)
[  794.261683] Filesystems sync: 0.000 seconds
[  794.270433] Freezing user space processes
[  794.276492] Freezing user space processes completed (elapsed 0.001 seconds)
[  794.283511] OOM killer disabled.
[  794.286770] Freezing remaining freezable tasks
[  794.292385] Freezing remaining freezable tasks completed (elapsed 0.001 seconds)
[  794.299800] printk: Suspending console(s) (use no_console_suspend to debug)
[  794.338802] ti-sci 44043000.system-controller: ti_sci_cmd_set_device_constraint: device: 179: state: 1: ret 0
[  794.338994] ti-sci 44043000.system-controller: ti_sci_cmd_set_device_constraint: device: 178: state: 1: ret 0
[  794.353412] ti-sci 44043000.system-controller: ti_sci_cmd_set_device_constraint: device: 117: state: 1: ret 0
[  794.361972] ti-sci 44043000.system-controller: ti_sci_suspend_noirq: Saving gpio ctx dir = |5f9dffff| out = |80600000|
[  794.362736] Disabling non-boot CPUs ...
[  794.364514] psci: CPU1 killed (polled 0 ms)
[  794.367999] psci: CPU2 killed (polled 0 ms)
[  794.371351] psci: CPU3 killed (polled 0 ms)
[  794.372492] Enabling non-boot CPUs ...
[  794.372945] Detected VIPT I-cache on CPU1
[  794.373010] GICv3: CPU1: found redistributor 1 region 0:0x00000000018a0000
[  794.373081] CPU1: Booted secondary processor 0x0000000001 [0x410fd034]
[  794.374455] CPU1 is up
[  794.374745] Detected VIPT I-cache on CPU2
[  794.374777] GICv3: CPU2: found redistributor 2 region 0:0x00000000018c0000
[  794.374823] CPU2: Booted secondary processor 0x0000000002 [0x410fd034]
[  794.375822] CPU2 is up
[  794.376110] Detected VIPT I-cache on CPU3
[  794.376147] GICv3: CPU3: found redistributor 3 region 0:0x00000000018e0000
[  794.376206] CPU3: Booted secondary processor 0x0000000003 [0x410fd034]
[  794.377545] CPU3 is up
[  794.378047] ti-sci 44043000.system-controller: ti_sci_resume: restoring gpio ctx dir = |5f9dffff| out = |80600000|
[  794.378160] ti-sci 44043000.system-controller: ti_sci_resume: wakeup source: 0x50
[  794.395455] am65-cpsw-nuss 8000000.ethernet: set new flow-id-base 19
[  794.406338] am65-cpsw-nuss 8000000.ethernet eth0: PHY [8000f00.mdio:00] driver [TI DP83867] (irq=368)
[  794.406981] am65-cpsw-nuss 8000000.ethernet eth0: configuring for phy/rgmii-rxid link mode
[  794.408281] usb-conn-gpio connector: repeated role: device
[  794.670158] OOM killer enabled.
[  794.673305] Restarting tasks ... done.
[  794.679377] random: crng reseeded on system resumption
[  794.684647] PM: suspend exit
root@verdin-am62-15412844:~# 
root@verdin-am62-15412844:~# rtcwake -s 10 -m mem -d rtc1
rtcwake: assuming RTC uses UTC ...
rtcwake: wakeup from "mem" using rtc1 at Thu Jan  1 00:14:24 1970
[  805.769552] PM: suspend entry (deep)
[  805.773477] Filesystems sync: 0.000 seconds
[  805.782090] Freezing user space processes
[  805.788075] Freezing user space processes completed (elapsed 0.001 seconds)
[  805.795122] OOM killer disabled.
[  805.798384] Freezing remaining freezable tasks
[  805.804352] Freezing remaining freezable tasks completed (elapsed 0.001 seconds)
[  805.811766] printk: Suspending console(s) (use no_console_suspend to debug)
[  805.840307] ti-sci 44043000.system-controller: ti_sci_cmd_set_device_constraint: device: 179: state: 1: ret 0
[  805.840509] ti-sci 44043000.system-controller: ti_sci_cmd_set_device_constraint: device: 178: state: 1: ret 0
[  805.853310] ti-sci 44043000.system-controller: ti_sci_cmd_set_device_constraint: device: 117: state: 1: ret 0
[  805.861803] ti-sci 44043000.system-controller: ti_sci_suspend_noirq: Saving gpio ctx dir = |5f9dffff| out = |80600000|
[  805.862558] Disabling non-boot CPUs ...
[  805.865161] psci: CPU1 killed (polled 4 ms)
[  805.868263] psci: CPU2 killed (polled 4 ms)
[  805.871443] psci: CPU3 killed (polled 0 ms)
[  805.872481] Enabling non-boot CPUs ...
[  805.872947] Detected VIPT I-cache on CPU1
[  805.873010] GICv3: CPU1: found redistributor 1 region 0:0x00000000018a0000
[  805.873084] CPU1: Booted secondary processor 0x0000000001 [0x410fd034]
[  805.874476] CPU1 is up
[  805.874765] Detected VIPT I-cache on CPU2
[  805.874796] GICv3: CPU2: found redistributor 2 region 0:0x00000000018c0000
[  805.874839] CPU2: Booted secondary processor 0x0000000002 [0x410fd034]
[  805.875919] CPU2 is up
[  805.876232] Detected VIPT I-cache on CPU3
[  805.876268] GICv3: CPU3: found redistributor 3 region 0:0x00000000018e0000
[  805.876320] CPU3: Booted secondary processor 0x0000000003 [0x410fd034]
[  805.877502] CPU3 is up
[  805.878014] ti-sci 44043000.system-controller: ti_sci_resume: restoring gpio ctx dir = |5f9dffff| out = |80600000|
[  805.878126] ti-sci 44043000.system-controller: ti_sci_resume: wakeup source: 0x50
[  805.895159] am65-cpsw-nuss 8000000.ethernet: set new flow-id-base 19
[  805.906080] am65-cpsw-nuss 8000000.ethernet eth0: PHY [8000f00.mdio:00] driver [TI DP83867] (irq=368)
[  805.906767] am65-cpsw-nuss 8000000.ethernet eth0: configuring for phy/rgmii-rxid link mode
[  805.908077] usb-conn-gpio connector: repeated role: device
[  806.169431] OOM killer enabled.
[  806.172580] Restarting tasks ... done.
[  806.178467] random: crng reseeded on system resumption
[  806.183748] PM: suspend exit
root@verdin-am62-15412844:~# 
root@verdin-am62-15412844:~# rtcwake -s 10 -m mem -d rtc1
rtcwake: assuming RTC uses UTC ...
rtcwake: wakeup from "mem" using rtc1 at Thu Jan  1 00:14:40 1970
[  811.913248] PM: suspend entry (deep)
[  811.917234] Filesystems sync: 0.000 seconds
[  811.922748] Freezing user space processes
[  811.928418] Freezing user space processes completed (elapsed 0.001 seconds)
[  811.935495] OOM killer disabled.
[  811.938763] Freezing remaining freezable tasks
[  811.944798] Freezing remaining freezable tasks completed (elapsed 0.001 seconds)
[  811.952209] printk: Suspending console(s) (use no_console_suspend to debug)
[  811.989693] ti-sci 44043000.system-controller: ti_sci_cmd_set_device_constraint: device: 179: state: 1: ret 0
[  811.989886] ti-sci 44043000.system-controller: ti_sci_cmd_set_device_constraint: device: 178: state: 1: ret 0
[  812.001309] ti-sci 44043000.system-controller: ti_sci_cmd_set_device_constraint: device: 117: state: 1: ret 0
[  812.009866] ti-sci 44043000.system-controller: ti_sci_suspend_noirq: Saving gpio ctx dir = |5f9dffff| out = |80600000|
[  812.010624] Disabling non-boot CPUs ...
[  812.013257] psci: CPU1 killed (polled 0 ms)
[  812.016168] psci: CPU2 killed (polled 4 ms)
[  812.019365] psci: CPU3 killed (polled 0 ms)
[  812.020584] Enabling non-boot CPUs ...
[  812.021045] Detected VIPT I-cache on CPU1
[  812.021106] GICv3: CPU1: found redistributor 1 region 0:0x00000000018a0000
[  812.021176] CPU1: Booted secondary processor 0x0000000001 [0x410fd034]
[  812.022561] CPU1 is up
[  812.022844] Detected VIPT I-cache on CPU2
[  812.022876] GICv3: CPU2: found redistributor 2 region 0:0x00000000018c0000
[  812.022920] CPU2: Booted secondary processor 0x0000000002 [0x410fd034]
[  812.023988] CPU2 is up
[  812.024690] Detected VIPT I-cache on CPU3
[  812.024737] GICv3: CPU3: found redistributor 3 region 0:0x00000000018e0000
[  812.024798] CPU3: Booted secondary processor 0x0000000003 [0x410fd034]
[  812.026021] CPU3 is up
[  812.026530] ti-sci 44043000.system-controller: ti_sci_resume: restoring gpio ctx dir = |5f9dffff| out = |80600000|
[  812.026643] ti-sci 44043000.system-controller: ti_sci_resume: wakeup source: 0x50
[  812.043811] am65-cpsw-nuss 8000000.ethernet: set new flow-id-base 19
[  812.054759] am65-cpsw-nuss 8000000.ethernet eth0: PHY [8000f00.mdio:00] driver [TI DP83867] (irq=368)
[  812.055398] am65-cpsw-nuss 8000000.ethernet eth0: configuring for phy/rgmii-rxid link mode
[  812.056695] usb-conn-gpio connector: repeated role: device
[  812.321287] OOM killer enabled.
[  812.324442] Restarting tasks ... done.
[  812.329622] random: crng reseeded on system resumption
[  812.334959] PM: suspend exit
root@verdin-am62-15412844:~# 

I assume the patch provided was more of a temporary solution for testing?
Will there be a solution that will be pushed in the firmware?

Thank you,

Franz