This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

J722SXH01EVM: Does vision_apps of J722SXH01EVM support csitx/dsitx, and how to enable it?

Part Number: J722SXH01EVM


Tool/software:

Hi experts,

I uesed J722SXH01EVM to test csitx/dsitx in vision_apps.

1. I found that gDssDisplayInterface is defined as DSS_HDMI_INTERFACE in generated/ti_drivers_config.c

In psdkra/vision_apps/platform/j722s/rtos/mcu2_0/generated/ti_drivers_config.h, there are two dss defination and  no relevant definition about DSS_DSI.

uint32_t gDssDisplayInterface = DSS_HDMI_INTERFACE;
#define DSS_HDMI_INTERFACE (0U)
#define DSS_OLDI_INTERFACE (1U)
#define DSS_MAX_INTERFACES (2U)

2. In psdkra/vision_apps/platform/j722s/rtos/common/app_cfg_mcu2_0.h

There's no mention of supporting DSS_DSI.

When ENABLE_DSS_SINGLE is defined, only one of ENABLE_DSS_HDMI or ENABLE_DSS_EDP should be defined
When ENABLE_DSS_DUAL is defined, ENABLE_DSS_HDMI and ENABLE_DSS_EDP are not used, both EDP and HDMI are enabled unconditionally

    /* IMPORANT NOTE:
     * - Only one of ENABLE_DSS_SINGLE or ENABLE_DSS_DUAL should be defined
     * - When ENABLE_DSS_SINGLE is defined, only one of ENABLE_DSS_HDMI or ENABLE_DSS_EDP should be defined
     * - When ENABLE_DSS_DUAL is defined, ENABLE_DSS_HDMI and ENABLE_DSS_EDP are not used, both EDP and HDMI are enabled unconditionally
     */
    #define ENABLE_DSS_SINGLE
    #undef  ENABLE_DSS_DUAL



version:

sdk rtos: ti-processor-sdk-rtos-j722s-evm-10_00_00_05.tar.gz

sdk linux: ti-processor-sdk-linux-adas-j722s-evm-10_00_00_08-Linux-x86-Install.bin

So, Does j722s's vision_apps  support DSS-DSI, and how to enable and test it.?