Other Parts Discussed in Thread: TMS320C6678
Hello,
I would like to do simulation of DDR3 interface for our designing C6678 board.
Now, I'm checking IBIS file of C6678 and found many models for this interface.
Regarding TX model for address and data line, I think **ohms mean setting of driver strength(resister which is connected between PTV15 and GND).
Our board is based on EVM, so we will use 45.3ohms.
In this case, should we use "TX 45ohms ..." model?
Regarding RX model for address and data line, some termination models are defined.
I'm not sure what this termination means.
(ODT or external termination?)
Could you explain about these termination settings?
Thanks,