This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AMIC110: Which floating-point hardware supporting on AMIC110?

Genius 3186 points

Part Number: AMIC110

Tool/software:

Hello,

May I question about AMIC110 CA8 hardware of floating point?

In GCC compiler, it supporting many format/hardware of floating point.

Such as auto’, ‘vfpv2’, ‘vfpv3’, ‘vfpv3-fp16’, ‘vfpv3-d16’, ‘vfpv3-d16-fp16’, ‘vfpv3xd’, ‘vfpv3xd-fp16’, ‘neon-vfpv3’, ‘neon-fp16’, ‘vfpv4’, ‘vfpv4-d16’, ‘fpv4-sp-d16’, ‘neon-vfpv4’, ‘fpv5-d16’, ‘fpv5-sp-d16’, ‘fp-armv8’, ‘neon-fp-armv8’ and ‘crypto-neon-fp-armv8’.

However, if build in CCS with starterware libraries, It may not allowed "auto".

Which is supporting?

I believe this question be depend on hardware so it avable E2E support.

Best regards,

GR