This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM3352: Impact when only VDD_MPU is OPP50 (0.95V)

Part Number: AM3352

Tool/software:

Our customer has encountered an error when the power supply voltages are set for AM3352BZCZ30 as follows:

VDD_CORE: OPP100 (1.1V)
VDD_MPU: OPP50 (0.95V)

The ARM (A8) is always running at 300 MHz due to the AM3352BZCZ30.

Are functions other than the ARM (A8) core also affected and limited when only VDD_MPU is OPP50 (0.95V)?

Do the OPP50 limitations on the datasheet also apply when only VDD_MPU is OPP50 (0.95V)?

Best regards,

Daisuke