This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM365 RMAN segmentation fault



I have segmentation fault while creating a codec such as H.264, JPEG, and dm365resizer on DM365.

 

Segmentation Fault in VISA_create2().

CE_DEBUG logs are as follows:

@3,409,011us: [+0 T:0x4001faf0 S:0xbea99804] ti.sdo.ce.osal.LockMP - Entered LockMP_release>lock[0x159bb8]
@3,409,214us: [+0 T:0x4001faf0 S:0xbea997e4] ti.sdo.ce.osal.SemMP - Entered SemMP_post> sem[0x159160]
@3,409,425us: [+0 T:0x4001faf0 S:0xbea997e4] ti.sdo.ce.osal.SemMP - Leaving SemMP_post> sem[0x159160]
@3,409,630us: [+0 T:0x4001faf0 S:0xbea9981c] ti.sdo.ce.osal.LockMP - Leaving LockMP_release>lock[0x159bb8]
@3,409,824us: [+7 T:0x4001faf0 S:0xbea9981c] ti.sdo.fc.rman - RMAN_assignResources> resFxns->initResources() failed [3]

 

S/W configuration is as follows:

Custom board 

Kernel Ver: 2.6.18

DVSDK Ver: 2.10.01.18

CE Ver: 2.24

FC Ver: 2.25.00.04

IPNC SW: custom SW

PSP Ver: LSP2.10, MV Pro 5.0

I've tried DVSDK 2.26.00.01, but have same problem(DVSDK 2.26.00.01 fixed segmentation error).

Thanks.