This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320C6672: NDK static ip

Other Parts Discussed in Thread: TMS320C6672

부품 번호: TMS320C6672

도구/소프트웨어:

Hello, I am using the hua_evmc6678l project of mcsdk_2_01_02_06.
When the project was uploaded to RAM for debugging, the IP was set as a static IP.
However, when running the project again without resetting the board's power, a problem occurred in which the static IP was not set.

I think that once the IP is set and the network is added, it must be released.
However, when I run it again, I don't know how to release the originally set IP.
Please tell me the reason and solution.