This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VEN-Q1: J722S :: TIDL Kernel Init Failed

Part Number: TDA4VEN-Q1

Tool/software:

Dear Sir,

I am working with

PSDK 9.2

OS : RTOS + LINUX

Below is the test pipeline

Camera- > Color Conversion -> Scalar -> Pre-processing -> TIDL 

I am using the existing TIDL Node, but it is failing at runtime

Error Code :

    41.749237 s:  VX_ZONE_ERROR:[ownContextSendCmd:875] Command ack message returned failure cmd_status: -1
    41.749281 s:  VX_ZONE_ERROR:[ownNodeKernelInit:590] Target kernel, TIVX_CMD_NODE_CREATE failed for node tidl_node
    41.749299 s:  VX_ZONE_ERROR:[ownNodeKernelInit:591] Please be sure the target callbacks have been registered for this core
    41.749310 s:  VX_ZONE_ERROR:[ownNodeKernelInit:592] If the target callbacks have been registered, please ensure no errors are occurring within the create callback of this kernel
    41.749323 s:  VX_ZONE_ERROR:[ownGraphNodeKernelInit:608] kernel init for node 6, kernel com.ti.tidl:1:3 ... failed !!!
    41.749364 s:  VX_ZONE_ERROR:[vxVerifyGraph:2170] Node kernel init failed
    41.749375 s:  VX_ZONE_ERROR:[vxVerifyGraph:2224] Graph verify failed

Please let me know If I am missing something.

Thanks and Regards,

Vyom Mishra