Part Number: AM4378
Tool/software:
Linux SDK: 07.03.00.005
USB0 connects a WIFI module. ESD cause the USB disconnecting. reset the external WIFI alone, can't re-enumerate
There are two fail mode different a little:
1: After ESD fail, replug USB WIFI module, can recognize product ID, but can't enumerate.
#2. After ESD fail, replug USB WIFI module, can't recognize product ID, can't enumerate.
Software reboot the system can resume USB and USB WIFI.
Ask How to reset the USB module to recover other than reboot the whole software.