Hi,
Environment:
AAC-HE Decoder version v1.30 on DM6467T with dvsdk version dvsdk_3_10_00_16.
I am facing issue while decoding ISO/IEC 14496-3 Audio with the LATM transport syntax as defined in ISO/IEC 14496-3 / AMD 1 aac files.
Please let me know if the aac decoder will be able to decode LATM complaint aac streams?
PFA aac file FYR.
Regards,
Sreeni.4336.test.txt