Part Number: AM3354
Tool/software:
Kernel V3.12.10
USB0 connects a USB to UART device, if disconnect the cable after application opened the device, Kernel sometimes crash.
Further experiments figured out if the USB_VBUS is disconnected before DP/DM during unplug can reproduce the failure easily.
Although the USB_VBUS pin is longer than other pins in connector, but it still can't ensure USB_VBUS is the last pin to be disconnected.
Question: Is it a known issue of the old Kernel? Is there specific fix for this issue In the old Kernel or later new SDK?