Hi,
I rotate the display by 90 degrees by setting "Angle" to 1 in dss.reg and it is fine. However, I have an external touch monitor that could not detect this rotation. To look into this issue, I ran the Xaml application "Bounce.xaml" and found out that XamlPerf.exe in BSP ARM_A8_01_01 also could not detect the rotation - the function call "ChangeDisplaySettingsEx(NULL, &DevMode, NULL, CDS_TEST, NULL)" in the file main.c of XAMLPERF always return DMDO_0 even though my display is rotated by 90 degrees.
Can you tell if it is a WinCE or BSP problem? I appreciate your help.
Luan