Seagate 570G ST3500418AS HD can not be worked on DM8168's SATA drive.
http://www.seagate.com/ww/v/index.jsp?vgnextoid=c501895c8ccce110VgnVCM100000f5ee0a0aRCRD
have any one know this issue ?
ThanKs
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Seagate 570G ST3500418AS HD can not be worked on DM8168's SATA drive.
http://www.seagate.com/ww/v/index.jsp?vgnextoid=c501895c8ccce110VgnVCM100000f5ee0a0aRCRD
have any one know this issue ?
ThanKs
I use UDWork Box V0.3A & RDK1508, ti8168_dvr_defconfig.
The console message :
ata2: SATA link up 3.0 Gbps (SStatus 123 SControl 300)
ata2.15: Port Multiplier 1.2, 0x197b:0x3215 r0, 5 ports, feat 0x5/0xf
ata2.00: hard resetting link
ata2.00: SATA link down (SStatus 0 SControl 320)
ata2.01: hard resetting link
ata2.01: SATA link down (SStatus 0 SControl 320)
ata2.02: hard resetting link
ata2.02: SATA link down (SStatus 0 SControl 320)
ata2.03: hard resetting link
ata2.03: SATA link down (SStatus 0 SControl 320)
ata2.04: hard resetting link
ata2.04: SATA link down (SStatus 0 SControl 320)
ata2: EH complete
ata1: softreset failed (1st FIS failed)
ata1: SATA link up 3.0 Gbps (SStatus 123 SControl 300)
ata1: link online but 1 devices misclassified, retrying
ata1: softreset failed (1st FIS failed)
ata1: SATA link up 3.0 Gbps (SStatus 123 SControl 300)
ata1: link online but 1 devices misclassified, retrying
ata1: softreset failed (1st FIS failed)
ata1: SATA link up 3.0 Gbps (SStatus 123 SControl 300)
ata1: link online but 1 devices misclassified, retrying
ata1: limiting SATA link speed to 1.5 Gbps
ata1: SATA link down (SStatus 1 SControl 310)