Part Number: AM620-Q1
Other Parts Discussed in Thread: UNIFLASH
Tool/software:
Hello Team,
I am working with the AM62x processor and came across advisory i2310 in the errata(i2371) document, which states that the ROM code may hang during UART boot mode due to a potential erroneous timeout interrupt. The workaround presented in advisory i2310 is not implemented in ROM, which can result in the ROM hanging when this issue occurs.
I Seeking some clarification on the following points:
1.Since the software workaround is not implemented in ROM, is there a recommended procedure to avoid or handle this issue during UART boot, especially when using UniFlash tool ?
2. Could you provide more details on the conditions that can trigger the erroneous timeout interrupt in UART boot mode?
Thanks,
Yashwanth