Tool/software:
Hello, I trained a model based on edgeai_yolov5, and then set "export TIDL_RT_ONNX_VARDIM=1" to complete the compilation of the model (using edgeai_benckmark). However, when I used the compiled model to run on the AM62A board, an error occurred. The error message was kernel init for node 0, kernel com.ti.tidl:1:3 ... failed !!!. I will upload the error log and the model file I used, and hope to get your reply and answer. Thank you.file0918.zip