Other Parts Discussed in Thread: OMAP3530, SYSCONFIG, ADS7846
Hi everyone;
i am working on OMAP 35x Evaluation Board. I want to run hello program in getting started on my board. And many times ı try but ı couldn't...
i write log files of my minicom screen. My nfshost ip address is 192.168.1.110. and ı connected omap board and host via router.
Problem is i couldn't connect omap board and nfshost.. So i couldn't access hello file on omap board
Thank you for help
xxxxxxxxxx--------------------------------------------------------xxxxxxxxxxxxxxxx--------------------------------------------
Texas Instruments X-Loader 1.42
Starting OS Bootloader...
No OOB scheme defined for oobsize 0
OneNAND: 0 kB
256 MiB
U-Boot 2008.10 (Sep 14 2009 - 13:40:58)
OMAP35X-Family-GP rev 2, CPU-OPP2 L3-165MHz
OMAP3 EVM board + LPDDR/NAND
In: serial
Out: serial
Err: serial
Hit any key to stop autoboot: 6 0
OMAP3_EVM # printenv
baudrate=115200
netmask=255.255.254.0
bootfile="uImage"
get_kernel=run nand_kernel
get_initrd=run nand_initrd
nand_kernel=nand read.i 0x80000000 280000 220000
nand_initrd=nand read.i 0x81600000 780000 1000000
tftp_kernel=tftpboot 0x80000000 uImage
tftp_initrd=tftpboot 0x81600000 ramdisk.gz
bootargs_rd=mem=128M console=ttyS0,115200n8 root=/dev/ram0 initrd=0x81600000,40M ramdisk_size=40960
bootargs_fs=mem=99M console=ttyS0,115200n8 noinitrd root=/dev/mtdblock4 rw rootfstype=jffs2 mpurate=600 omapfb.rotate=1 omapfb.rotate_type=1 omap_vout.vid1_static_vrfb_alloc=y
addip=setenv bootargs $(bootargs) ip=$(ipaddr):$(serverip):$(gatewayip):$(netmask):$(hostname):eth0:on
boot_rd=run get_kernel; run get_initrd; setenv bootargs $(bootargs_rd); run addip; bootm 0x80000000
boot_fs=run get_kernel; setenv bootargs $(bootargs_fs); bootm 0x80000000
boot_nfs=run get_kernel; setenv bootargs $(bootargs_nfs); run addip; bootm 0x80000000
bootdelay=6
ethaddr=00:50:C2:7E:90:C9
ipaddr=172.19.243.95
nfshost193.140.48.53=193.140.48.53
rootpath=/home/agumuscu/workdir/filesys
bootcmd=run boot_nfs
nfshost2=192.168.1.110
bootargs_nfs=console=ttyS0,115200n8 noinitrd rw ip=dhcp root=/dev/nfs nfsroot=192.168.1.110:/home/agumuscu/workdir/filesys,nolock mem=99M mpurate=600 omapfb.rotate=1 omapfb.rotate_type=1 omap_vout.vid1_static_vrfb_alloc=y
stdin=serial
stdout=serial
stderr=serial
Environment size: 1409/131068 bytes
OMAP3_EVM # boot
NAND read: device 0 offset 0x280000, size 0x220000
2228224 bytes read: OK
## Booting kernel from Legacy Image at 80000000 ...
Image Name: Linux-2.6.29-rc3-omap1
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 2128064 Bytes = 2 MB
Load Address: 80008000
Entry Point: 80008000
Verifying Checksum ... OK
Loading Kernel Image ... OK
OK
Starting kernel ...
Uncompressing Linux........................................................................................................................................... done, booting the kernel.
<5>Linux version 2.6.29-rc3-omap1 (x0029463@psplinux050) (gcc version 4.2.3 (Sourcery G++ Lite 2008q1-126)) #1 Mon Sep 14 13:51:49 IST 2009
CPU: ARMv7 Processor [411fc083] revision 3 (ARMv7), cr=10c5387f
CPU: VIPT nonaliasing data cache, VIPT nonaliasing instruction cache
Machine: OMAP3 EVM
Memory policy: ECC disabled, Data cache writeback
<7>On node 0 totalpages: 25344
<7>free_area_init_node: node 0, pgdat c0440c24, node_mem_map c0464000
<7> Normal zone: 198 pages used for memmap
<7> Normal zone: 0 pages reserved
<7> Normal zone: 25146 pages, LIFO batch:7
<6>OMAP3530 ES3.1 (full speed SGX, IVA2)
<6>SRAM: Mapped pa 0x40200000 to va 0xd7000000 size: 0x100000
Built 1 zonelists in Zone order, mobility grouping on. Total pages: 25146
<5>Kernel command line: console=ttyS0,115200n8 noinitrd rw ip=dhcp root=/dev/nfs nfsroot=192.168.1.110:/home/agumuscu/workdir/filesys,nolock mem=99M mpurate=600 omapfb.rotate=1 omapfb.rotate_type=1 omap_vout.vid1_static_vrfb_alloc=y ip=172.19.243.95:::255.255.254.0::eth0:on
<6>Clocking rate (Crystal/DPLL/MPU core): 26.0/332/500 MHz
<6>IVA2 clocking rate: 360 MHz
<6>Reprogramming SDRC
<6>GPMC revision 5.0
<6>IRQ: Found an INTC at 0xd8200000 (revision 4.0) with 96 interrupts
<6>Total of 96 interrupts on 1 active controller
<6>OMAP34xx GPIO hardware version 2.5
PID hash table entries: 512 (order: 9, 2048 bytes)
<6>OMAP clockevent source: GPTIMER1 at 32768 Hz
Console: colour dummy device 80x30
<6>Dentry cache hash table entries: 16384 (order: 4, 65536 bytes)
<6>Inode-cache hash table entries: 8192 (order: 3, 32768 bytes)
<6>Memory: 99MB = 99MB total
<5>Memory: 95800KB available (3928K code, 370K data, 156K init)
<6>Calibrating delay loop... 499.92 BogoMIPS (lpj=1949696)
Mount-cache hash table entries: 512
<6>CPU: Testing write buffer coherency: ok
<6>net_namespace: 520 bytes
<6>NET: Registered protocol family 16
<4>MUX: setup AF26_34XX_GPIO0 (0xd80021e0): 0x011c -> 0x0118
<4>MUX: setup L8_34XX_GPIO63 (0xd80020ce): 0x0118 -> 0x0004
<4>MUX: setup AF9_34XX_GPIO22 (0xd80025ec): 0x0100 -> 0x011c
<4>MUX: setup U3_34XX_GPIO61 (0xd80020c8): 0x0118 -> 0x011c
<4>MUX: setup AH14_34XX_GPIO21 (0xd80025ea): 0x0100 -> 0x011c
<4>MUX: setup AA10_3430_USB2HS_PHY_STP (0xd80025f2): 0x0100 -> 0x0003
<4>MUX: setup AA8_3430_USB2HS_PHY_CLK (0xd80025f0): 0x0100 -> 0x0003
<4>MUX: setup AA9_3430_USB2HS_PHY_DIR (0xd80025f4): 0x0100 -> 0x010b
<4>MUX: setup AB11_3430_USB2HS_PHY_NXT (0xd80025f6): 0x0100 -> 0x010b
<4>MUX: setup AB10_3430_USB2HS_PHY_D0 (0xd80025f8): 0x0100 -> 0x010b
<4>MUX: setup AB9_3430_USB2HS_PHY_D1 (0xd80025fa): 0x0100 -> 0x010b
<4>MUX: setup W3_3430_USB2HS_PHY_D2 (0xd80021d4): 0x0108 -> 0x010b
<4>MUX: setup T4_3430_USB2HS_PHY_D3 (0xd80021de): 0x0108 -> 0x010b
<4>MUX: setup T3_3430_USB2HS_PHY_D4 (0xd80021d8): 0x0100 -> 0x010b
<4>MUX: setup R3_3430_USB2HS_PHY_D5 (0xd80021da): 0x0100 -> 0x010b
<4>MUX: setup R4_3430_USB2HS_PHY_D6 (0xd80021dc): 0x0108 -> 0x010b
<4>MUX: setup T2_3430_USB2HS_PHY_D7 (0xd80021d6): 0x0100 -> 0x010b
<3>twl4030: client 1 is not initialized
<3>twl4030: client 1 is not initialized
<4>MUX: setup AA21_34XX_GPIO157 (0xd800218e): 0x0018 -> 0x011c
<4>MUX: setup C23_34XX_GPIO98 (0xd8002114): 0x0004 -> 0x011c
<6>omap3evmdc: Driver registration complete
<6>Switched to new clocking rate (Crystal/Core/MPU): 26.0/332/600 MHz
<6>IVA2 clocking rate: 430 MHz
<6>Calibrating delay loop... 597.64 BogoMIPS (lpj=2334720)
<6>OMAP DMA hardware revision 4.0
<3>USB: No board-specific platform config found
<6>OMAP DSS rev 2.0
<6>OMAP DISPC rev 3.0
<6>OMAP VENC rev 2
<6>OMAP DSI rev 1.0
bio: create slab <bio-0> at 0
<6>i2c_omap i2c_omap.1: bus 1 rev3.12 at 2600 kHz
<6>twl4030: PIH (irq 7) chaining IRQs 368..375
<6>twl4030: power (irq 373) chaining IRQs 376..383
<6>twl4030: gpio (irq 368) chaining IRQs 384..401
<6>i2c_omap i2c_omap.2: bus 2 rev3.12 at 400 kHz
<6>i2c_omap i2c_omap.3: bus 3 rev3.12 at 400 kHz
<5>SCSI subsystem initialized
<6>usbcore: registered new interface driver usbfs
<6>usbcore: registered new interface driver hub
<6>usbcore: registered new device driver usb
<6>musb_hdrc: version 6.0, musb-dma, host, debug=0
<7>HS USB OTG: revision 0x33, sysconfig 0x2011, sysstatus 0x1, intrfsel 0x1, simenable 0x0
<7>musb_hdrc: ConfigData=0xde (UTMI-8, dyn FIFOs, bulk combine (X), bulk split (X), HB-ISO Rx (X), HB-ISO Tx (X), SoftConn)
<7>musb_hdrc: MHDRC RTL version 1.400
<7>musb_hdrc: setup fifo_mode 4
<7>musb_hdrc: 29/31 max ep, 16384/16384 memory
<7>musb_hdrc: hw_ep 0shared, max 64
<7>musb_hdrc: hw_ep 1tx, max 512
<7>musb_hdrc: hw_ep 1rx, max 512
<7>musb_hdrc: hw_ep 2tx, max 512
<7>musb_hdrc: hw_ep 2rx, max 512
<7>musb_hdrc: hw_ep 3tx, max 512
<7>musb_hdrc: hw_ep 3rx, max 512
<7>musb_hdrc: hw_ep 4tx, max 512
<7>musb_hdrc: hw_ep 4rx, max 512
<7>musb_hdrc: hw_ep 5tx, max 512
<7>musb_hdrc: hw_ep 5rx, max 512
<7>musb_hdrc: hw_ep 6tx, max 512
<7>musb_hdrc: hw_ep 6rx, max 512
<7>musb_hdrc: hw_ep 7tx, max 512
<7>musb_hdrc: hw_ep 7rx, max 512
<7>musb_hdrc: hw_ep 8tx, max 512
<7>musb_hdrc: hw_ep 8rx, max 64
<7>musb_hdrc: hw_ep 9tx, max 512
<7>musb_hdrc: hw_ep 9rx, max 64
<7>musb_hdrc: hw_ep 10tx, max 512
<7>musb_hdrc: hw_ep 10rx, max 64
<7>musb_hdrc: hw_ep 11tx, max 256
<7>musb_hdrc: hw_ep 11rx, max 256
<7>musb_hdrc: hw_ep 12tx, max 256
<7>musb_hdrc: hw_ep 12rx, max 256
<7>musb_hdrc: hw_ep 13tx, max 256
<7>musb_hdrc: hw_ep 13rx, max 4096
<7>musb_hdrc: hw_ep 14shared, max 1024
<7>musb_hdrc: hw_ep 15shared, max 1024
<6>musb_hdrc: USB Host mode controller at d80ab000 using DMA, IRQ 92
<6>musb_hdrc musb_hdrc: MUSB HDRC host driver
<6>musb_hdrc musb_hdrc: new USB bus registered, assigned bus number 1
<6>usb usb1: New USB device found, idVendor=1d6b, idProduct=0002
<6>usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
<6>usb usb1: Product: MUSB HDRC host driver
<6>usb usb1: Manufacturer: Linux 2.6.29-rc3-omap1 musb-hcd
<6>usb usb1: SerialNumber: musb_hdrc
<6>usb usb1: configuration #1 chosen from 1 choice
<6>hub 1-0:1.0: USB hub found
<6>hub 1-0:1.0: 1 port detected
<7>Registered /proc/driver/musb_hdrc
<6>NET: Registered protocol family 2
<7>Switched to high resolution mode on CPU 0
<6>IP route cache hash table entries: 1024 (order: 0, 4096 bytes)
<6>TCP established hash table entries: 4096 (order: 3, 32768 bytes)
<6>TCP bind hash table entries: 4096 (order: 2, 16384 bytes)
<6>TCP: Hash tables configured (established 4096 bind 4096)
<6>TCP reno registered
<6>NET: Registered protocol family 1
<6>OMAP35x Linux PSP version 02.01.03.11 (OMAP3EVM)
<4>NetWinder Floating Point Emulator V0.97 (double precision)
<5>VFS: Disk quotas dquot_6.5.2
Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
<6>JFFS2 version 2.2. (NAND) © 2001-2006 Red Hat, Inc.
<6>msgmni has been set to 187
<6>alg: No test for stdrng (krng)
<6>io scheduler noop registered
<6>io scheduler anticipatory registered (default)
<6>io scheduler deadline registered
<6>io scheduler cfq registered
Generic Backlight Driver Initialized.
<6>Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled
<6>serial8250.0: ttyS0 at MMIO 0x4806a000 (irq = 72) is a ST16654
<6>console [ttyS0] enabled
Linux version 2.6.29-rc3-omap1 (x0029463@psplinux050) (gcc version 4.2.3 (Sourcery G++ Lite 2008q1-126)) #1 Mon Sep 14 13:51:49 IST 2009
CPU: ARMv7 Processor [411fc083] revision 3 (ARMv7), cr=10c5387f
CPU: VIPT nonaliasing data cache, VIPT nonaliasing instruction cache
Machine: OMAP3 EVM
Memory policy: ECC disabled, Data cache writeback
OMAP3530 ES3.1 (full speed SGX, IVA2)
SRAM: Mapped pa 0x40200000 to va 0xd7000000 size: 0x100000
Built 1 zonelists in Zone order, mobility grouping on. Total pages: 25146
Kernel command line: console=ttyS0,115200n8 noinitrd rw ip=dhcp root=/dev/nfs nfsroot=192.168.1.110:/home/agumuscu/workdir/filesys,nolock mem=99M mpurate=600 omapfb.rotate=1 omapfb.rotate_type=1 omap_vout.vid1_static_vrfb_alloc=y ip=172.19.243.95:::255.255.254.0::eth0:on
Clocking rate (Crystal/DPLL/MPU core): 26.0/332/500 MHz
IVA2 clocking rate: 360 MHz
Reprogramming SDRC
GPMC revision 5.0
IRQ: Found an INTC at 0xd8200000 (revision 4.0) with 96 interrupts
Total of 96 interrupts on 1 active controller
OMAP34xx GPIO hardware version 2.5
PID hash table entries: 512 (order: 9, 2048 bytes)
OMAP clockevent source: GPTIMER1 at 32768 Hz
Console: colour dummy device 80x30
Dentry cache hash table entries: 16384 (order: 4, 65536 bytes)
Inode-cache hash table entries: 8192 (order: 3, 32768 bytes)
Memory: 99MB = 99MB total
Memory: 95800KB available (3928K code, 370K data, 156K init)
Calibrating delay loop... 499.92 BogoMIPS (lpj=1949696)
Mount-cache hash table entries: 512
CPU: Testing write buffer coherency: ok
net_namespace: 520 bytes
NET: Registered protocol family 16
MUX: setup AF26_34XX_GPIO0 (0xd80021e0): 0x011c -> 0x0118
MUX: setup L8_34XX_GPIO63 (0xd80020ce): 0x0118 -> 0x0004
MUX: setup AF9_34XX_GPIO22 (0xd80025ec): 0x0100 -> 0x011c
MUX: setup U3_34XX_GPIO61 (0xd80020c8): 0x0118 -> 0x011c
MUX: setup AH14_34XX_GPIO21 (0xd80025ea): 0x0100 -> 0x011c
MUX: setup AA10_3430_USB2HS_PHY_STP (0xd80025f2): 0x0100 -> 0x0003
MUX: setup AA8_3430_USB2HS_PHY_CLK (0xd80025f0): 0x0100 -> 0x0003
MUX: setup AA9_3430_USB2HS_PHY_DIR (0xd80025f4): 0x0100 -> 0x010b
MUX: setup AB11_3430_USB2HS_PHY_NXT (0xd80025f6): 0x0100 -> 0x010b
MUX: setup AB10_3430_USB2HS_PHY_D0 (0xd80025f8): 0x0100 -> 0x010b
MUX: setup AB9_3430_USB2HS_PHY_D1 (0xd80025fa): 0x0100 -> 0x010b
MUX: setup W3_3430_USB2HS_PHY_D2 (0xd80021d4): 0x0108 -> 0x010b
MUX: setup T4_3430_USB2HS_PHY_D3 (0xd80021de): 0x0108 -> 0x010b
MUX: setup T3_3430_USB2HS_PHY_D4 (0xd80021d8): 0x0100 -> 0x010b
MUX: setup R3_3430_USB2HS_PHY_D5 (0xd80021da): 0x0100 -> 0x010b
MUX: setup R4_3430_USB2HS_PHY_D6 (0xd80021dc): 0x0108 -> 0x010b
MUX: setup T2_3430_USB2HS_PHY_D7 (0xd80021d6): 0x0100 -> 0x010b
twl4030: client 1 is not initialized
twl4030: client 1 is not initialized
MUX: setup AA21_34XX_GPIO157 (0xd800218e): 0x0018 -> 0x011c
MUX: setup C23_34XX_GPIO98 (0xd8002114): 0x0004 -> 0x011c
omap3evmdc: Driver registration complete
Switched to new clocking rate (Crystal/Core/MPU): 26.0/332/600 MHz
IVA2 clocking rate: 430 MHz
Calibrating delay loop... 597.64 BogoMIPS (lpj=2334720)
OMAP DMA hardware revision 4.0
USB: No board-specific platform config found
OMAP DSS rev 2.0
OMAP DISPC rev 3.0
OMAP VENC rev 2
OMAP DSI rev 1.0
bio: create slab <bio-0> at 0
i2c_omap i2c_omap.1: bus 1 rev3.12 at 2600 kHz
twl4030: PIH (irq 7) chaining IRQs 368..375
twl4030: power (irq 373) chaining IRQs 376..383
twl4030: gpio (irq 368) chaining IRQs 384..401
i2c_omap i2c_omap.2: bus 2 rev3.12 at 400 kHz
i2c_omap i2c_omap.3: bus 3 rev3.12 at 400 kHz
SCSI subsystem initialized
usbcore: registered new interface driver usbfs
usbcore: registered new interface driver hub
usbcore: registered new device driver usb
musb_hdrc: version 6.0, musb-dma, host, debug=0
musb_hdrc: USB Host mode controller at d80ab000 using DMA, IRQ 92
musb_hdrc musb_hdrc: MUSB HDRC host driver
musb_hdrc musb_hdrc: new USB bus registered, assigned bus number 1
usb usb1: New USB device found, idVendor=1d6b, idProduct=0002
usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
usb usb1: Product: MUSB HDRC host driver
usb usb1: Manufacturer: Linux 2.6.29-rc3-omap1 musb-hcd
usb usb1: SerialNumber: musb_hdrc
usb usb1: configuration #1 chosen from 1 choice
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 1 port detected
NET: Registered protocol family 2
IP route cache hash table entries: 1024 (order: 0, 4096 bytes)
TCP established hash table entries: 4096 (order: 3, 32768 bytes)
TCP bind hash table entries: 4096 (order: 2, 16384 bytes)
TCP: Hash tables configured (established 4096 bind 4096)
TCP reno registered
NET: Registered protocol family 1
OMAP35x Linux PSP version 02.01.03.11 (OMAP3EVM)
NetWinder Floating Point Emulator V0.97 (double precision)
VFS: Disk quotas dquot_6.5.2
Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
JFFS2 version 2.2. (NAND) © 2001-2006 Red Hat, Inc.
msgmni has been set to 187
alg: No test for stdrng (krng)
io scheduler noop registered
io scheduler anticipatory registered (default)
io scheduler deadline registered
io scheduler cfq registered
Generic Backlight Driver Initialized.
Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled
serial8250.0: ttyS0 at MMIO 0x4806a000 (irq = 72) is a ST16654
console [ttyS0] enabled
<6>serial8250.0: ttyS1 at MMIO 0x4806c000 (irq = 73) is a ST16654
serial8250.0: ttyS1 at MMIO 0x4806c000 (irq = 73) is a ST16654
<6>serial8250.0: ttyS2 at MMIO 0x49020000 (irq = 74) is a ST16654
serial8250.0: ttyS2 at MMIO 0x49020000 (irq = 74) is a ST16654
<6>brd: module loaded
brd: module loaded
<6>loop: module loaded
loop: module loaded
<6>smsc911x: Driver version 2008-10-21.
smsc911x: Driver version 2008-10-21.
<6>smsc911x-mdio: probed
smsc911x-mdio: probed
<6>eth0: attached PHY driver [Generic PHY] (mii_bus:phy_addr=ffffffff:01, irq=-1)
eth0: attached PHY driver [Generic PHY] (mii_bus:phy_addr=ffffffff:01, irq=-1)
<6>net eth0: MAC Address: 00:50:c2:7e:90:c9
net eth0: MAC Address: 00:50:c2:7e:90:c9
<6>Linux video capture interface: v2.00
Linux video capture interface: v2.00
<6>usbcore: registered new interface driver uvcvideo
usbcore: registered new interface driver uvcvideo
<6>USB Video Class driver (v0.1.0)
USB Video Class driver (v0.1.0)
<6>i2c /dev entries driver
i2c /dev entries driver
<4>Driver 'sd' needs updating - please use bus_type methods
Driver 'sd' needs updating - please use bus_type methods
<6>omap2-nand driver initializing
omap2-nand driver initializing
<6>NAND device: Manufacturer ID: 0x2c, Chip ID: 0xba (Micron NAND 256MiB 1,8V 16-bit)
NAND device: Manufacturer ID: 0x2c, Chip ID: 0xba (Micron NAND 256MiB 1,8V 16-bit)
<5>Creating 5 MTD partitions on "omap2-nand.0":
Creating 5 MTD partitions on "omap2-nand.0":
<5>0x000000000000-0x000000080000 : "xloader-nand"
0x000000000000-0x000000080000 : "xloader-nand"
<5>0x000000080000-0x000000240000 : "uboot-nand"
0x000000080000-0x000000240000 : "uboot-nand"
<5>0x000000240000-0x000000280000 : "params-nand"
0x000000240000-0x000000280000 : "params-nand"
<5>0x000000280000-0x000000780000 : "linux-nand"
0x000000280000-0x000000780000 : "linux-nand"
<5>0x000000780000-0x000010000000 : "jffs2-nand"
0x000000780000-0x000010000000 : "jffs2-nand"
<6>OneNAND driver initializing
OneNAND driver initializing
<6>ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
<6>ehci-omap ehci-omap.0: OMAP-EHCI Host Controller
ehci-omap ehci-omap.0: OMAP-EHCI Host Controller
<6>ehci-omap ehci-omap.0: new USB bus registered, assigned bus number 2
ehci-omap ehci-omap.0: new USB bus registered, assigned bus number 2
<6>ehci-omap ehci-omap.0: irq 77, io mem 0x48064800
ehci-omap ehci-omap.0: irq 77, io mem 0x48064800
<6>ehci-omap ehci-omap.0: USB 2.0 started, EHCI 1.00
ehci-omap ehci-omap.0: USB 2.0 started, EHCI 1.00
<6>usb usb2: New USB device found, idVendor=1d6b, idProduct=0002
usb usb2: New USB device found, idVendor=1d6b, idProduct=0002
<6>usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1
usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1
<6>usb usb2: Product: OMAP-EHCI Host Controller
usb usb2: Product: OMAP-EHCI Host Controller
<6>usb usb2: Manufacturer: Linux 2.6.29-rc3-omap1 ehci_hcd
usb usb2: Manufacturer: Linux 2.6.29-rc3-omap1 ehci_hcd
<6>usb usb2: SerialNumber: ehci-omap.0
usb usb2: SerialNumber: ehci-omap.0
<6>usb usb2: configuration #1 chosen from 1 choice
usb usb2: configuration #1 chosen from 1 choice
<6>hub 2-0:1.0: USB hub found
hub 2-0:1.0: USB hub found
<6>hub 2-0:1.0: 3 ports detected
hub 2-0:1.0: 3 ports detected
<6>Initializing USB Mass Storage driver...
Initializing USB Mass Storage driver...
<6>usbcore: registered new interface driver usb-storage
usbcore: registered new interface driver usb-storage
<6>USB Mass Storage support registered.
USB Mass Storage support registered.
<6>input: omap_twl4030keypad as /class/input/input0
input: omap_twl4030keypad as /class/input/input0
<6>ads7846 spi1.0: touchscreen, irq 335
ads7846 spi1.0: touchscreen, irq 335
<6>input: ADS784x Touchscreen as /class/input/input1
input: ADS784x Touchscreen as /class/input/input1
<6>OMAP Watchdog Timer Rev 0x31: initial timeout 60 sec
OMAP Watchdog Timer Rev 0x31: initial timeout 60 sec
<6>cpuidle: using governor ladder
cpuidle: using governor ladder
<6>cpuidle: using governor menu
cpuidle: using governor menu
<6>usbcore: registered new interface driver usbhid
usbcore: registered new interface driver usbhid
<6>usbhid: v2.6:USB HID core driver
usbhid: v2.6:USB HID core driver
<6>Advanced Linux Sound Architecture Driver Version 1.0.19.
Advanced Linux Sound Architecture Driver Version 1.0.19.
<6>usbcore: registered new interface driver snd-usb-audio
usbcore: registered new interface driver snd-usb-audio
<4>No device for DAI twl4030
No device for DAI twl4030
<4>No device for DAI twl4030 Voice
No device for DAI twl4030 Voice
<4>No device for DAI omap-mcbsp-dai-0
No device for DAI omap-mcbsp-dai-0
<4>No device for DAI omap-mcbsp-dai-1
No device for DAI omap-mcbsp-dai-1
<4>No device for DAI omap-mcbsp-dai-2
No device for DAI omap-mcbsp-dai-2
<4>No device for DAI omap-mcbsp-dai-3
No device for DAI omap-mcbsp-dai-3
<4>No device for DAI omap-mcbsp-dai-4
No device for DAI omap-mcbsp-dai-4
<6>OMAP3 EVM SoC init
OMAP3 EVM SoC init
<6>TWL4030 Audio Codec init
TWL4030 Audio Codec init
<6>asoc: twl4030 <-> omap-mcbsp-dai-0 mapping ok
asoc: twl4030 <-> omap-mcbsp-dai-0 mapping ok
<6>ALSA device list:
ALSA device list:
<6> #0: omap3evm (twl4030)
#0: omap3evm (twl4030)
<6>TCP cubic registered
TCP cubic registered
<6>NET: Registered protocol family 17
NET: Registered protocol family 17
<6>NET: Registered protocol family 15
NET: Registered protocol family 15
<6>RPC: Registered udp transport module.
RPC: Registered udp transport module.
<6>RPC: Registered tcp transport module.
RPC: Registered tcp transport module.
<3>Power Management for TI OMAP3.
Power Management for TI OMAP3.
<6>SmartReflex driver initialized
SmartReflex driver initialized
<6>Disabling unused clock "sr2_fck"
Disabling unused clock "sr2_fck"
<6>Disabling unused clock "sr1_fck"
Disabling unused clock "sr1_fck"
<6>Disabling unused clock "mcbsp_fck"
Disabling unused clock "mcbsp_fck"
<6>Disabling unused clock "mcbsp_fck"
Disabling unused clock "mcbsp_fck"
<6>Disabling unused clock "mcbsp_fck"
Disabling unused clock "mcbsp_fck"
<6>Disabling unused clock "mcbsp_ick"
Disabling unused clock "mcbsp_ick"
<6>Disabling unused clock "mcbsp_ick"
Disabling unused clock "mcbsp_ick"
<6>Disabling unused clock "mcbsp_ick"
Disabling unused clock "mcbsp_ick"
<6>Disabling unused clock "gpt2_ick"
Disabling unused clock "gpt2_ick"
<6>Disabling unused clock "gpt3_ick"
Disabling unused clock "gpt3_ick"
<6>Disabling unused clock "gpt4_ick"
Disabling unused clock "gpt4_ick"
<6>Disabling unused clock "gpt5_ick"
Disabling unused clock "gpt5_ick"
<6>Disabling unused clock "gpt6_ick"
Disabling unused clock "gpt6_ick"
<6>Disabling unused clock "gpt7_ick"
Disabling unused clock "gpt7_ick"
<6>Disabling unused clock "gpt8_ick"
Disabling unused clock "gpt8_ick"
<6>Disabling unused clock "gpt9_ick"
Disabling unused clock "gpt9_ick"
<6>Disabling unused clock "wdt3_ick"
Disabling unused clock "wdt3_ick"
<6>Disabling unused clock "wdt3_fck"
Disabling unused clock "wdt3_fck"
<6>Disabling unused clock "gpio2_dbck"
Disabling unused clock "gpio2_dbck"
<6>Disabling unused clock "gpio3_dbck"
Disabling unused clock "gpio3_dbck"
<6>Disabling unused clock "gpio4_dbck"
Disabling unused clock "gpio4_dbck"
<6>Disabling unused clock "gpio5_dbck"
Disabling unused clock "gpio5_dbck"
<6>Disabling unused clock "gpt9_fck"
Disabling unused clock "gpt9_fck"
<6>Disabling unused clock "gpt8_fck"
Disabling unused clock "gpt8_fck"
<6>Disabling unused clock "gpt7_fck"
Disabling unused clock "gpt7_fck"
<6>Disabling unused clock "gpt6_fck"
Disabling unused clock "gpt6_fck"
<6>Disabling unused clock "gpt5_fck"
Disabling unused clock "gpt5_fck"
<6>Disabling unused clock "gpt4_fck"
Disabling unused clock "gpt4_fck"
<6>Disabling unused clock "gpt3_fck"
Disabling unused clock "gpt3_fck"
<6>Disabling unused clock "gpt2_fck"
Disabling unused clock "gpt2_fck"
<6>Disabling unused clock "gpt12_ick"
Disabling unused clock "gpt12_ick"
<6>Disabling unused clock "wdt1_ick"
Disabling unused clock "wdt1_ick"
<6>Disabling unused clock "wdt2_ick"
Disabling unused clock "wdt2_ick"
<6>Disabling unused clock "wdt2_fck"
Disabling unused clock "wdt2_fck"
<6>Disabling unused clock "gpio1_dbck"
Disabling unused clock "gpio1_dbck"
<6>Disabling unused clock "des1_ick"
Disabling unused clock "des1_ick"
<6>Disabling unused clock "sha11_ick"
Disabling unused clock "sha11_ick"
<6>Disabling unused clock "rng_ick"
Disabling unused clock "rng_ick"
<6>Disabling unused clock "aes1_ick"
Disabling unused clock "aes1_ick"
<6>Disabling unused clock "ssi_ick"
Disabling unused clock "ssi_ick"
<6>Disabling unused clock "mailboxes_ick"
Disabling unused clock "mailboxes_ick"
<6>Disabling unused clock "mcbsp_ick"
Disabling unused clock "mcbsp_ick"
<6>Disabling unused clock "mcbsp_ick"
Disabling unused clock "mcbsp_ick"
<6>Disabling unused clock "gpt10_ick"
Disabling unused clock "gpt10_ick"
<6>Disabling unused clock "gpt11_ick"
Disabling unused clock "gpt11_ick"
<6>Disabling unused clock "hdq_ick"
Disabling unused clock "hdq_ick"
<6>Disabling unused clock "mspro_ick"
Disabling unused clock "mspro_ick"
<6>Disabling unused clock "des2_ick"
Disabling unused clock "des2_ick"
<6>Disabling unused clock "sha12_ick"
Disabling unused clock "sha12_ick"
<6>Disabling unused clock "aes2_ick"
Disabling unused clock "aes2_ick"
<6>Disabling unused clock "icr_ick"
Disabling unused clock "icr_ick"
<6>Disabling unused clock "pka_ick"
Disabling unused clock "pka_ick"
<6>Disabling unused clock "ssi_ssr_fck"
Disabling unused clock "ssi_ssr_fck"
<6>Disabling unused clock "hdq_fck"
Disabling unused clock "hdq_fck"
<6>Disabling unused clock "mcbsp_fck"
Disabling unused clock "mcbsp_fck"
<6>Disabling unused clock "mcbsp_fck"
Disabling unused clock "mcbsp_fck"
<6>Disabling unused clock "mspro_fck"
Disabling unused clock "mspro_fck"
<6>Disabling unused clock "gpt11_fck"
Disabling unused clock "gpt11_fck"
<6>Disabling unused clock "sad2d_ick"
Disabling unused clock "sad2d_ick"
<6>Disabling unused clock "dpll4_m6x2_ck"
Disabling unused clock "dpll4_m6x2_ck"
<6>Disabling unused clock "dpll3_m3x2_ck"
Disabling unused clock "dpll3_m3x2_ck"
<6>Disabling unused clock "sys_clkout1"
Disabling unused clock "sys_clkout1"
<6>VFP support v0.3: VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 1
implementor 41 architecture 3 part 30 variant c rev 1
<4>GPIO-153 autorequested
GPIO-153 autorequested
<3>omap-dss DISPC error: Requested pixel clock not possible with the current OMAP2_DSS_MIN_FCK_PER_PCK setting. Turning the constraint off.
omap-dss DISPC error: Requested pixel clock not possible with the current OMAP2_DSS_MIN_FCK_PER_PCK setting. Turning the constraint off.
<4>omap-dss: Could not find exact pixel clock. Requested 25190 kHz, got 25189 kHz
omap-dss: Could not find exact pixel clock. Requested 25190 kHz, got 25189 kHz
<4>Display already enabled
Display already enabled
<4>Display already enabled
Display already enabled
<6>Buffer Size = 3686400
Buffer Size = 3686400
<6>omap_vout: registered and initialized video device 0 [v4l2]
omap_vout: registered and initialized video device 0 [v4l2]
<6>Buffer Size = 3686400
Buffer Size = 3686400
<6>omap_vout: registered and initialized video device 1 [v4l2]
omap_vout: registered and initialized video device 1 [v4l2]
<6>display->updated
display->updated
<6>net eth0: SMSC911x/921x identified at 0xc685c000, IRQ: 336
net eth0: SMSC911x/921x identified at 0xc685c000, IRQ: 336
IP-Config: Complete:IP-Config: Complete:
device=eth0
device=eth0, addr=172.19.243.95, addr=172.19.243.95, mask=255.255.254.0, mask=255.255.254.0, gw=255.255.255.255, gw=255.255.255.255,
host=172.19.243.95, domain=, nis-domain=(none),
host=172.19.243.95, domain=, nis-domain=(none),
bootserver=255.255.255.255,
bootserver=255.255.255.255, rootserver=192.168.1.110, rootserver=192.168.1.110, rootpath=, rootpath=
<5>Looking up port of RPC 100003/2 on 192.168.1.110
Looking up port of RPC 100003/2 on 192.168.1.110
<5>rpcbind: server 192.168.1.110 not responding, timed out
rpcbind: server 192.168.1.110 not responding, timed out
<3>Root-NFS: Unable to get nfsd port number from server, using default
Root-NFS: Unable to get nfsd port number from server, using default
<5>Looking up port of RPC 100005/1 on 192.168.1.110
Looking up port of RPC 100005/1 on 192.168.1.110
<5>rpcbind: server 192.168.1.110 not responding, timed out
rpcbind: server 192.168.1.110 not responding, timed out
<3>Root-NFS: Unable to get mountd port number from server, using default
Root-NFS: Unable to get mountd port number from server, using default
<3>Root-NFS: Server returned error -5 while mounting /home/agumuscu/workdir/filesys
Root-NFS: Server returned error -5 while mounting /home/agumuscu/workdir/filesys
<3>VFS: Unable to mount root fs via NFS, trying floppy.
VFS: Unable to mount root fs via NFS, trying floppy.
VFS: Cannot open root device "nfs" or unknown-block(2,0)
VFS: Cannot open root device "nfs" or unknown-block(2,0)
Please append a correct "root=" boot option; here are the available partitions:
Please append a correct "root=" boot option; here are the available partitions:
1f00 512 mtdblock01f00 512 mtdblock0 (driver?)
(driver?)
1f01 1792 mtdblock11f01 1792 mtdblock1 (driver?)
(driver?)
1f02 256 mtdblock21f02 256 mtdblock2 (driver?)
(driver?)
1f03 5120 mtdblock31f03 5120 mtdblock3 (driver?)
(driver?)
1f04 254464 mtdblock41f04 254464 mtdblock4 (driver?)
(driver?)
<0>Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(2,0)
Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(2,0)