Part Number: TDA4VE-Q1
Other Parts Discussed in Thread: AM69A
Tool/software:
Hi experts,
edgeai-tidl-tools Tag: 09_02_09_00
I use docker to implement.
Due to network issues, I downloaded all the required libraries in advance and placed them in path edgeai-tidl-tools/downloads_for_edgeai,The edgeai-tidl-tools/setup.sh file has also been modified accordingly,
Refer to the "setup.patch" file.
Another change is the installation of the Tensort code repository. I downloaded TensorRT-release-8.5zip in advance and renamed it to TensorRT. I placed it in the edgeai-tidl-tools/scripts/osmt_model_tools/onnx_tools/tidl-onnx-model-optizer path, and manually executed the pip3 install . in the TensorRT/tools/onnx-gradhsurgeon path.
The final installation was successful, but there was an error while executing “cmake ../examples && make -j && cd ..“. I tried several times but it was the same error, missing the relevant dynamic library.
Can you help me check which package these libraries are in? Is it because which step did not execute successfully that these libraries are missing?