Tool/software:
Hello TI,
We are trying to boot our custom board through the latest linux build version 10.00.00.08 but it is stuck at u-boot giving the following error:
U-Boot SPL 2024.04-ti-g818c76aed67f (Aug 01 2024 - 19:19:47 +0000) SYSFW ABI: 4.0 (firmware rev 0x000a '10.0.8--v10.00.08 (Fiery Fox)') SPL initial stack usage: 13568 bytes Trying to boot from MMC2 Authentication passed Authentication passed Authentication passed Authentication passed Authentication passed Starting ATF on ARM64 core... NOTICE: BL31: v2.10.0(release):v2.10.0-367-g00f1ec6b87-dirty NOTICE: BL31: Built : 16:09:05, Feb 9 2024 U-Boot SPL 2024.04-ti-g818c76aed67f (Aug 01 2024 - 19:19:47 +0000) SYSFW ABI: 4.0 (firmware rev 0x000a '10.0.8--v10.00.08 (Fiery Fox)') Trying to boot from MMC2 i2c_write: error waiting for data ACK (status=0x116) pca953x gpio@22: Error reading output register Error reading cluster spl_load_image_fat: error reading image u-boot.img, err - -22 SPL: failed to boot from all boot devices ### ERROR ### Please RESET the board ###
Also tried with the prebuild image file for the same.