Part Number: CCSTUDIO
Tool/software:
Hi guys,
I am trying to get used to CCS Theia....
Question1
Does any of you have a clue why the Watch window shows data in DEC format even through I specifically set the display format to HEX?
See the picture attached. It seems that this is related only when I watch the structure (e.g. adcDataA). I can see the HEX value when I go for adcDataA.status. (as also shown in the picture).
Question2
In CCS (Eclipse), I was very used to just selecting the variable in my source code, right click -> watch. This feature is missing. I have to manually type down the variable name. I won't even get any suggestions. Are there any plans to do something about it?
Just my observation:
CCS Theia feels like arduino IDE with many great features missing. It looks good but it feels extremely crippled.
Best regards, Jiri