This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OMAP L137 Linux SPI Slave

 We are building a device that requires the L137 to act as an SPI slave in communications.  We want the ARM (via Linux) to handle the SPI communications. I am using the Davinci SDK,  Arago Linux (Kernel 2.6.18).  Searching these forums and the web, I get mixed messages on whether or not it is possible to have a slave mode SPI under this Linux kernel and with the drivers available.   Is this true?   If not, what can I do?    Is there a simple tweak to the master driver that allows SPI slave mode to be used via user space as a character device?  Can someone help me tackle this problem?

 

More linux info:

# uname -a
Linux da830-omapl137-evm 2.6.18_pro500-da830_omapl137_evm-arm_v5t_le #1 PREEMPT Thu Apr 23 17:41:16 IST 2009 armv5tejl unknown