Other Parts Discussed in Thread: CODECOMPOSER
Hi Folks,
We would like to use the C5535 for a battery powered, I/O heavy application. There is an external ADC with SPI interface. We do 4 byte reads at 312,500 reads per second. SPI clock is 10MHz. transferring data to the DSP at 1,250,000 bytes/sec. After some simple nibble/byte packing and buffering, we write blocks of data to microSD flash at 937,500 bytes/sec.
We need to sustain these rates for at least 1 hour.
We just discovered that the C5535 DMA controller does not support the SPI interface. Surprise!
Any suggestions?
Mike