This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[FAQ] AM625 / AM623 / AM620-Q1 / AM62L / AM62Ax / AM62D-Q1 / AM62Px / AM64x / AM243x Design Recommendations / Custom board hardware design – Queries related to CAP_VDDSx CAP_VDDS

Part Number: AM625
Other Parts Discussed in Thread: AM62D-Q1, AM62L

Tool/software:

HI TI experts,

Could you provide recommendations on CAP_VDDSx, cap value and effect of the capacitor not mounted or shorted.

  • HI Board designers, 

    Recommendations on CAP_VDDSx value 

    The LDO specification is 0.8uF to 1.5uF.  The capacitor should be within this range, considering bias, degradation over time etc.

     Q. With a 6.3V cap selected, considering the DC effect and other degradation, the cap value could go down to 0.7 uF.  Higher cap value may call for using a 0402 cap and that could have an effect on the layout.

    Does the capacitance depend on number of IOs used for the specific IO supply rail and the IOs current source/sink  or irrespective of the IO usage, the capacitance is required.

    https://www.kyocera-avx.com/docs/techinfo/CeramicCapacitors/mlcc-dc-bias-characteristics.pdf

    https://community.infineon.com/t5/Knowledge-Base-Articles/DC-Bias-characteristics-of-Multilayer-Ceramic-Capacitor-MLCC/ta-p/250035#.

    The cap value is independent of IO count and activity. It is required for stability of the LDO to generate BIAS supply. Any value beyond this specified range could make BIAS generator unstable resulting in over voltage stress.

    Consider using a 10V or greater voltage rated cap to ensure the cap is within 0.8-1.5uF 

    Additional Guidelines 

    Select cap with less the 1 ohm ESR
    Ensure the PCB loop inductance is < 2.5 nH
    Use smallest possible (0201 or greater) package to minimize loop inductance
    Refer SoC Data sheet

    Regards,

    Sreenivasa

  • HI Board designers, 

     CAP_VDDSx voltage 

    It is not a fixed voltage. When the respective VDDSHV is operating at 1.8V, the pin should have the same potential as the VDDSHV source.

    When the respective VDDSHV is operating at 3.3V, it should have a potential that track to ½ of the VDDSHV source.

    When VDDSHV is ramping to 3.3V the LDO output will track VDDSHV until it gets up to about 2.4V. This is when bias supply circuit changes from what I call switch mode to LDO mode. At this point it begin to track ½ VDDSHV. I suspect the output capacitance will hold the 2.4V potential for a period of time before the IO bias circuits draw enough current to discharge the capacitor back down to the ½ VDDSHV potential.

    I would expect a similar thing to happen as the VDDSHV decays. When VDDSHV drops below 2.4V the bias supply circuit will switch back to switch mode, where the potential of VDDSHV is applied to the capacitor. 

    The CAP_VDDSn is optional when the IO group supply VDDSHVx is connected to 1.8V. When connected to 3.3V, the voltage to be considered for derating is the steady state DC output which is VDDSHVx/2. 

    Regards,

    Sreenivasa

  • HI Board designers, 

    Effect of the CAP_VDDSx on the SOC performance

    The capacitor is connected to the output of an internal LDO.  The LDO will not function correctly if the capacitor is not connected to this pin or if this pin is shorted to ground.  The LDO powers circuits in each IO buffer associated with the respective bank of IOs.  The IO buffers will not operate as expected if the LDO is not operating as expected.  If the LDO is not operating properly the IO buffer circuits may be permanently damaged.   Any SOC that has been exposed to a condition that prevents the LDO from operating as expected should be removed, discarded, and replaced with a new unit.

    Regards,

    Sreenivasa

  • HI Board designers, 

    Updates for AM62 capacitor connection (Valid for AM62x, AM62Ax, AM62D-Q1, AM62Px, AM64x, AM234x)

    AM62L supports 1.8V fixed voltage IOs and Dual-voltage fixed or dynamically switched IOs

    Caps are required for Dual-voltage IO supply for IO groups 

    CAP_VDDS_GENERAL1 CAP External capacitor connection for GENERAL1 IO group

    CAP_VDDS_GPMC External capacitor connection for GPMC IO group 
    CAP_VDDS_MMC0 External capacitor connection for MMC0 IO group 
    CAP_VDDS_MMC1 External capacitor connection for MMC1 IO group

    CAP_VDDS_MMC2 External capacitor connection for MMC2 IO group

    This pin must always be connected via a 6.3V or greater, 0.8uF to 1.5μF (Consider using a 10V or greater voltage rated cap to ensure the cap is within 0.8-1.5uF) capacitor to VSS if the respective VDDSHVx pin is ever operated at 3.3V IO supply. The capacitor selected must provide a capacitance within the defined range after considering tolerance DC-bias, operating temperature, and aging effects. There are three connection options if the respective VDDSHVx pin is only operated at 1.8V. The pin can be connected to the same decoupling capacitor that is required for 3.3V operation, it can be left unconnected, or it can be connected to the same 1.8V power source as the respective VDDSHVx pin.

    AM62L supports integrated LDO for powering the SD card interface (support UHS-I SD card)

    CAP_VDDSHV_MMC External capacitor connection for SDIO_LDO

    This pin must always be connected via a 6.3V or greater, 3.3μF ±20% capacitor to VSS when the SDIO_LDO is being used to source VDDSHV3 or VDDSHV4. The capacitor selected must provide a capacitance within the defined range after considering tolerance, DC-bias, operating temperature, and aging effects. Otherwise, this pin may be connected directly to VSS when the VDDA_3P3_SDIO pin is also connected directly to VSS.

    Regards,

    Sreenivasa

  • HI Board designers, 

    Additional inputs:

     I would like to know what would be the affects to the SoC/system if any of the below CAPs were missing or of an incorrect value. 

    * Capacitor is optional when the VDDSHVx IO supply group is connected to 1,8V

    Note on capacitor choice:

    Use capacitors with tolerance of ±10%
    Use cap with voltage rating of 10V or higher considering DC bias
    Select capacitor with ESR < 1 ohm
    Ensure the PCB loop inductance is < 2.5 nH
    Select 0201 package or smallest possible package nearest to 0201

    Example part number 

    CL03A105KP3NSNC
    1 µF ±10% 10V Ceramic Capacitor X5R 0201 (0603 Metric)

    GRM155R61A105KE15D
    SMD Multilayer Ceramic Capacitor, 1 µF, 10 V, 0402 [1005 Metric], ± 10%, X5R

    These capacitors are connected to internal LDOs that power IO bias circuits. They are required to maintain LDO stability. If you tried to operate the device without these capacitors, the LDO could become unstable and produce an unexpected output voltage that may damage the circuits in all IO cells associated with that bank of IOs.

    The CAP_VDDS pins are connected to the output of respective internal bias generators (LDOs) for each bank of IOs. Separate external capacitor are required to maintain a stable bias supply for the respective bank of IOs. The equivalent VDDSHV pin(s) are used to power the respective bank of IOs and its internal bias generator. So effectively the VDDSHV supply is the input to the internal bias generator and the equivalent CAP_VDDS pin is the output of the internal bias generator. So the VDDSHV power pins still need their own decoupling capacitors.

    When not mounted, you would likely see functional failures since these caps are required for the internal LDOs to regulate to the correct voltage.

    Regards,

    Sreenivasa