Part Number: AM62P
Tool/software:
We wish to use crystal P/N: Q22FA1280071000 [ FA-128 case 2016 25MHz 6pF 10ppm , 30ppm -40+85C , 80 Ohm ESR] (datasheet attached) for our AM62P design.
1. I went over the AM62P datasheet section requirements listed in Table 6-21 but it is not clear if Cshunt requirement will be met, can you check if Q22FA1280071000 meets the crystal requirements?
2. Selection of CL1,CL2 caps - The PROC164E1-1 reference schematics shows using XRCGB25M000F3A00R0 which has Load Capacitance of 6pF and the CL1/CL2 caps used with it C47,C50 are 18pF.
Attempting to calculate for example C47, According to datasheet, CL1 = [(2CL) - (CPCBXI + CXI)] =[(2x6) - CPCBXI - 1.58] = [12 - CPCBXI - 1.58] = [10.42 - CPCBXI] which is less than 18pF
a. Can you explain the calculation?
b. What would be the recommended baseline for CL1/CL2 when using Q22FA1280071000?
John