Tool/software:
Hi
I am trying to validate the sleep mode in the EVM using the command echo mem > /sys/power/state. It seems the EVM is going into sleep mode as per below logs and also on power supply I could see the drop of current consumption by approx 6mA as soon the command is given. Can you let me know how to resume the EVM back from the sleep state?
Also on pressing the WARM switch at SW9 the current consumption further reduces to approx 20mA. Can you please let me know the functionality of this switch?
The SDK version for J784S4 is 10_00_00_08 & boot mode is eMMC.
Thanks,
Arjav Parikh